ZHCSEX3A February   2016  – March  2016 TPS22918

PRODUCTION DATA.  

  1. 1 特性
  2. 2 应用
  3. 3 说明
  4. 4 修订历史记录
  5. 5 Pin Configuration and Functions
  6. 6 Specifications
    1. 6.1 Absolute Maximum Ratings
    2. 6.2 ESD Ratings
    3. 6.3 Recommended Operating Conditions
    4. 6.4 Thermal Information
    5. 6.5 Electrical Characteristics
    6. 6.6 Switching Characteristics
    7. 6.7 Typical Characteristics
      1. 6.7.1 DC Characteristics
      2. 6.7.2 AC Characteristics
  7. 7 Parameter Measurement Information
  8. 8 Detailed Description
    1. 8.1 Overview
    2. 8.2 Functional Block Diagram
    3. 8.3 Feature Description
      1. 8.3.1 On and Off Control
      2. 8.3.2 Quick Output Discharge (QOD)
        1. 8.3.2.1 QOD when System Power is Removed
        2. 8.3.2.2 Internal QOD Considerations
      3. 8.3.3 Adjustable Rise Time (CT)
    4. 8.4 Device Functional Modes
  9. 9 Application and Implementation
    1. 9.1 Application Information
    2. 9.2 Typical Application
      1. 9.2.1 Design Requirements
      2. 9.2.2 Detailed Design Procedure
        1. 9.2.2.1 Input Capacitor (CIN)
        2. 9.2.2.2 Output Capacitor (CL) (Optional)
        3. 9.2.2.3 Shutdown Sequencing During Unexpected System Power Loss
        4. 9.2.2.4 VIN to VOUT Voltage Drop
        5. 9.2.2.5 Inrush Current
      3. 9.2.3 Application Curves
  10. 10Power Supply Recommendations
  11. 11Layout
    1. 11.1 Layout Guidelines
    2. 11.2 Layout Example
    3. 11.3 Thermal Considerations
  12. 12器件和文档支持
    1. 12.1 器件支持
      1. 12.1.1 开发支持
    2. 12.2 文档支持
      1. 12.2.1 相关文档 
    3. 12.3 社区资源
    4. 12.4 商标
    5. 12.5 静电放电警告
    6. 12.6 Glossary
  13. 13机械、封装和可订购信息

9 Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

9.1 Application Information

This section highlights some of the design considerations when implementing this device in various applications. A PSPICE model for this device is also available in the product page of this device on www.ti.com (See the 器件支持 section for more information).

9.2 Typical Application

This typical application demonstrates how the TPS22918 can be used to power downstream modules.

TPS22918 final block2.png Figure 23. Typical Application Schematic

9.2.1 Design Requirements

For this design example, use the values listed in Table 5 as the design parameters:

Table 5. Design Parameters

DESIGN PARAMETER EXAMPLE VALUE
VIN 5 V
Load Current 2 A
CL 22 µF
Desired Fall Time 4 ms
Maximum Acceptable Inrush Current 400 mA

9.2.2 Detailed Design Procedure

9.2.2.1 Input Capacitor (CIN)

To limit the voltage drop on the input supply caused by transient in-rush currents when the switch turns on into a discharged load capacitor or short-circuit, a capacitor needs to be placed between VIN and GND. A 1 µF ceramic capacitor, CIN, placed close to the pins, is usually sufficient. Higher values of CIN can be used to further reduce the voltage drop during high-current application. When switching heavy loads, it is recommended to have an input capacitor about 10 times higher than the output capacitor to avoid excessive voltage drop.

9.2.2.2 Output Capacitor (CL) (Optional)

Becuase of the integrated body diode in the MOSFET, a CIN greater than CL is highly recommended. A CL greater than CIN can cause VOUT to exceed VIN when the system supply is removed. This could result in current flow through the body diode from VOUT to VIN. A CIN to CL ratio of 10 to 1 is recommended for minimizing VIN dip caused by inrush currents during startup.

9.2.2.3 Shutdown Sequencing During Unexpected System Power Loss

Microcontrollers and processors often have a specific shutdown sequence in which power needs to be removed. Using the adjustable Quick Output Discharge function of the TPS22918, adding a load switch to each power rail can be used to manage the power down sequencing in the event of an unexpected system power loss (i.e. battery removal). To determine the QOD values for each load switch, first confirm the power down order of the device you wish to power sequence. Be sure to check if there are voltage or timing margins that must be maintained during power down. Next, consult QOD Fall Time Table in the Quick Output Discharge (QOD) feature description to determine appropriate COUT and RQOD values for each power rail's load switch so that the load switches' fall times correspond to the order in which they need to be powered down. In the above example, we would like this power rail's fall time to be 4 ms. Using Equation 2, to determine the appropriate RQOD to achieve our desired fall time.
Because fall times are measured from 90% of VOUT to 10% of VOUT, the equation becomes:

Equation 4. .5 V = 4.5 V × e-(4 ms) / (R × (22 µF))
Equation 5. RQOD = 83.333 Ω

Refer to Figure 7, RPD at VIN = 5 V is approximately 25 Ω. Using Equation 1, the required external QOD resistance can be calculated:

Equation 6. 83.333 Ω = 25 Ω + REXT
Equation 7. REXT = 58.333 Ω

Figure 24 through Figure 29 are scope shots demonstrating an example of the QOD functionality when power is removed from the device (both ON and VIN are disconnected simultaneously). The input voltage is decaying in all scope shots below.

  • Initial VIN = 3.3 V
  • QOD = Open, 500 Ω, or shorted to VOUT
  • CL = 1 μF, 10 μF
  • VOUT is left floating

NOTE: VIN may appear constant in some figures. This is because the time scale of the scope shot is too small to show the decay of CIN.

TPS22918 tFall with QOD_CIN=COUT=1uF_VIN=3.3V_QOD=Open.png
A.
VIN = 3.3 V CIN = 1 µF CL = 1 µF
QOD = Open
Figure 24. tF at VIN = 3.3 V
TPS22918 tFall with QOD_CIN=COUT=1uF_VIN=3.3V_QOD=VOUT.png
A.
VIN = 3.3 V CIN = 1 µF CL = 1 µF
QOD = VOUT
Figure 26. tF at VIN = 3.3 V
TPS22918 tFall with QOD_CIN=COUT=10uF_VIN=3.3V_QOD=500ohm_zommed out.png
A.
VIN = 3.3 V CIN = 1 µF CL = 10 µF
QOD = 500 Ω
Figure 28. tF at VIN = 3.3 V
TPS22918 tFall with QOD_CIN=COUT=1uF_VIN=3.3V_QOD=500ohm.png
A.
VIN = 3.3 V CIN = 1 µF CL = 1 µF
QOD = 500 Ω
Figure 25. tF at VIN = 3.3 V
TPS22918 tFall with QOD_CIN=COUT=10uF_VIN=3.3V_QOD=Open.png
A.
VIN = 3.3 V CIN = 1 µF CL = 10 µF
QOD = Open
Figure 27. tF at VIN = 3.3 V
TPS22918 tFall with QOD_CIN=COUT=10uF_VIN=3.3V_QOD=VOUT_zoomed out.png
A.
VIN = 3.3 V CIN = 1 µF CL = 10 µF
QOD = VOUT
Figure 29. tF at VIN = 3.3 V

9.2.2.4 VIN to VOUT Voltage Drop

The VIN to VOUT voltage drop in the device is determined by the RON of the device and the load current. The RON of the device depends upon the VIN conditions of the device. Refer to the RON specification of the device in the Electrical Characteristics table of this data sheet. When the RON of the device is determined based upon the VIN conditions, use Equation 8 to calculate the VIN to VOUT voltage drop:

Equation 8. ∆V = ILOAD × RON

where

  • ΔV = voltage drop from VIN to VOUT
  • ILOAD = load current
  • RON = On-resistance of the device for a specific VIN

9.2.2.5 Inrush Current

Use Equation 9 to determine how much inrush current will be caused by the CL capacitor:

Equation 9. TPS22918 Q3_Iinhush_slvsco0.gif

where

  • IINRUSH = amount of inrush caused by CL
  • CL = capacitance on VOUT
  • dt = Output Voltage rise time during the ramp up of VOUT when the device is enabled
  • dVOUT = change in VOUT during the ramp up of VOUT when the device is enabled

The appropriate rise time can be calculated using the design requirements and the inrush current equation. As we are calculating the rise time (measured from 10% to 90% of VOUT), we will account for this in our dVOUT parameter (80% of VOUT = 4 V).

Equation 10. 400 mA = 22 μF × 4 V/dt
Equation 11. dt = 220 μs

To ensure an inrush current of less than 400 mA, choose a CT value that will yield a rise time of more than 220 μs. Consulting Table 2 at VIN = 5 V, CT = 220 μF will provide a typical rise time of 650 μs. Inputting this rise time and voltage into Equation 9, yields:

Equation 12. IInrush = 22 μF × 4 V / 650 μs
Equation 13. IInrush = 135 mA

This inrush current can be seen in the Application Curves below. An appropriate CL value should be placed on VOUT such that the IMAX and IPLS specifications of the device are not violated.

9.2.3 Application Curves

TPS22918 beforeinrush.png
VIN = 5 V CL = 22 µF CT = 0 µF
Figure 30. TPS22918 Inrush Current
TPS22918 afterinrush.png
VIN = 5 V CL = 22 µF CT = 220 µF
Figure 31. TPS22918 Inrush Current