ZHCSDT6 May 2015 LM36922
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The LM36922 provides a complete high-performance LED lighting solution for mobile handsets. The LM36922 is highly configurable and can support multiple LED configurations.
Figure 32. LM36922 Typical Application
| DESIGN PARAMETER | EXAMPLE VALUE |
|---|---|
| Minimum input voltage (VIN) | 2.7 V |
| LED parallel/series configuration | 2 × 8 |
| LED maximum forward voltage (Vf) | 3.2 V |
| Efficiency | 80% |
The number of LED strings, number of series LEDs, and minimum input voltage are needed in order to calculate the peak input current. This information guides the designer to make the appropriate inductor selection for the application. The LM36922 boost converter output voltage (VOUT) is calculated as follows: number of series LEDs × Vƒ + 0.23 V. The LM36922 boost converter output current (IOUT) is calculated as follows: number of parallel LED strings × 25 mA. The LM36922 peak input current is calculated using Equation 6.
The LM36922 requires a typical inductance in the range of 10 µH to 22 µH. When selecting the inductor, ensure that the saturation rating for the inductor is high enough to accommodate the peak inductor current of the application (IPEAK) given in the inductor datasheet. The peak inductor current occurs at the maximum load current, the maximum output voltage, the minimum input voltage, and the minimum switching frequency setting. Also, the peak current requirement increases with decreasing efficiency. IPEAK can be estimated using Equation 6:

Also, the peak current calculated above is different from the peak inductor current setting (ISAT). The NMOS switch current limit setting (ICL_MIN) must be greater than IPEAK from Equation 6 above.
The LM36922 requires a ceramic capacitor with a minimum of 0.4 µF of capacitance at the output, specified over the entire range of operation. This ensures that the device remains stable and oscillation free. The 0.4 µF of capacitance is the minimum amount of capacitance, which is different than the value of capacitor. Capacitance would take into account tolerance, temperature, and DC voltage shift.
Table 21 lists possible output capacitors that can be used with the LM36922. Figure 33 shows the DC bias of the four TDK capacitors. The useful voltage range is determined from the effective output voltage range for a given capacitor as determined by Equation 7:

| PART NUMBER | MANUFACTURER | CASE SIZE | VOLTAGE RATING (V) | NOMINAL CAPACITANCE (µF) | TOLERANCE (%) | TEMPERATURE COEFFICIENT (%) | RECOMMENDED MAX OUTPUT VOLTAGE (FOR SINGLE CAPACITOR) |
|---|---|---|---|---|---|---|---|
| C2012X5R1H105K085AB | TDK | 0805 | 50 | 1 | ±10 | ±15 | 22 |
| C2012X5R1H225K085AB | TDK | 0805 | 50 | 2.2 | ±10 | ±15 | 24 |
| C1608X5R1V225K080AC | TDK | 0603 | 35 | 2.2 | ±10 | ±15 | 12 |
| C1608X5R1H105K080AB | TDK | 0603 | 50 | 1 | ±10 | ±15 | 15 |
For example, with a 10% tolerance, and a 15% temperature coefficient, the DC voltage derating must be ≥ 0.38/(0.9 × 0.85) = 0.5 µF. For the C1608X5R1H225K080AB (0603, 50-V) device, the useful voltage range occurs up to the point where the DC bias derating falls below 0.523 µF, or around 12 V. For configurations where VOUT is > 15 V, two of these capacitors can be paralleled, or a larger capacitor such as the C2012X5R1H105K085AB must be used.
Figure 33. DC Bias Derating for 0805 Case Size andThe input capacitor in a boost is not as critical as the output capacitor. The input capacitor primary function is to filter the switching supply currents at the device input and to filter the inductor current ripple at the input of the inductor. The recommended input capacitor is a 2.2-µF ceramic (0402, 10-V device) or equivalent.
Figure 34. Boost Efficiency vs Series LEDs
Figure 35. Boost Efficiency vs Series LEDs
Figure 36. Boost Efficiency vs Series LEDs
Figure 38. Boost Efficiency vs Series LEDs
Figure 40. Boost Efficiency vs Series LEDs
Figure 42. Boost Efficiency vs Series LEDs
Figure 44. LED Current vs Brightness Code
Figure 46. LED Matching (Linear Mapping)
Figure 48. LED Current Accuracy
Figure 50. LED Headroom Voltage (Mis-Matched Strings)
Figure 37. Boost Efficiency vs Series LEDs
Figure 39. Boost Efficiency vs Series LEDs
Figure 41. Boost Efficiency vs Series LEDs
Figure 43. LED Current vs Brightness Code (Exponential Mapping)
Figure 45. LED Matching (Exponential Mapping)
Figure 47. LED Current Accuracy
Figure 49. LED Headroom Voltage (Mis-Matched Strings)
Figure 51. Current vs PWM Sample Frequency