ZHCSDR2A April 2015 – October 2024 FDC1004-Q1
PRODUCTION DATA
The capacitance measurement registers are 24-bit result registers in binary format (the 8 LSBs D[7:0] are always 0x00). The result of the acquisition is always a 24 bit value, while the accuracy is related to the selected conversion time (refer to ). The data is encoded in a Two’s complement format. The result of the measurement can be calculated by the following formula:
where