SSZTD60B October 2024 – September 2025 REF80 , REF81
Precision test equipment relies on precise data converters to make sure that any measurements taken accurately represent the device under test. For test and measurement, any offset error, gain error or decrease in the effective number of bits negatively affects the measurements generated. Unfortunately, however, it’s not possible to design all of these errors out of a high-precision system. Things like temperature drift or long-term drift eventually present themselves in the form of a gain or offset error. For this reason, calibration must occur to make sure that any measurements taken are accurate.
For calibration to be effective, there must be unchanging voltage levels available. Colloquially, you can call this a “golden reference.” As the analog-to-digital converter (ADC) measures these known voltage levels, the ADC compares the results and uses any differences to determine the gain and offset error. Figure 1 illustrates an example configuration of this circuit.
After quantifying the gain and offset error, software can compensate for the difference. This method of calibration is essential to maintaining accurate measurements for test applications, and is totally reliant on the golden reference, which gets as close to unchanging as possible. Of course, no circuit is completely unchanging, so even a highly precise voltage reference does exhibit small amounts of drift with time.
A golden reference that shifts with time affects the entire system’s accuracy. Parameters of a golden reference that affect system accuracy include long-term drift, temperature drift and noise.
Selecting a voltage reference that minimizes the errors caused by the parameters listed in Table 1 leads to the selection of a buried Zener voltage reference that has an internal heater. Buried Zener voltage references provide a voltage level that drifts minimally with time and temperature and has ultra-low noise. An example of such a device is the REF80 from TI. Table 1 also includes some REF80 performance specifications.
| Voltage reference parameter | Specification |
|---|---|
| Long-term drift | 3ppm (0 to 1000 hours) 0.3ppm (1000 to 5000 hours) |
| Temperature drift | 0.05ppm/°C typical 0.2ppm/°C maximum |
| 0.1Hz to 10Hz noise | 0.12ppmp-p |
0.1Hz to 10Hz noise and temperature drift affect the output of the voltage reference, therefore leading to calibration errors. The most important specification to consider for calibration is long-term drift, however, because that is the parameter that directly affects how often you need to calibrate the entire system.
When calibrating ADCs and DACs throughout test and measurement equipment, a buried Zener voltage reference helps determine how the ADC and DAC output values have shifted. And although buried Zener voltage references shift very little with time, in high-precision test equipment you must still account for even small variations in the output voltage. Many test and measurement systems require calibrating the golden reference after a number of months to confirm that system calibration dependent on the golden reference remains accurate. Figure 2 shows the long-term drift of the REF80.
There are a few important aspects of Figure 2 that demonstrates why the REF80 is a good fit for the calibration of highly precise test and measurement systems. First, most of the output voltage drift happens in the first 400 hours, of device operation. This is important, because the quicker the output voltage drift settles, the less there is a need for calibration because the output voltage does not drift nearly as much. In other words, the decrease in long-term drift also decreases the number of calibrations needed. For a parametric measurement unit in automated test equipment, this outcome is especially pertinent (see Figure 3).
Automated test equipment must be calibrated after a certain number of months to confirm that the golden reference output voltage drift has not affected the precision of the tester measurements. Each time calibration occurs, the entire system must go offline, which costs time and money. Using a buried Zener voltage reference such as the REF80 decreases the time needed for and cost of calibration.
If your design calls for a calibration voltage or reference voltage other than 7.6V, which is the output voltage of REF80, you can consider the REF81. The REF81 device has a buried Zener voltage output of 7.6V, but also integrates an internal buffer and precision resistor divider inside of the heated device to generate an additional low-drift output voltage. An example of how REF81 is used to generate multiple output voltages can be seen in Figure 4.
REF81 also has an option to configure the buffer to provide a gain of two for the output voltage. This means that if you are using the 5V version of REF81, you can configure the device such that the buffer has an output voltage of 10V.
Using the REF80 or REF81 with advanced calibration methods can allow precise test and measurement applications to maintain accurate for as long as possible. Without precision the likes of what REF80 and REF81 can produce, test and measurement systems fail to provide the necessary results to keep advanced electronics on the path of progression. As we strive to do our best to usher in a new era of precision, devices like the REF80 and REF81 can lead the way.
All trademarks are the property of their respective owners.