SSZTCB7 august   2015 LM5160

 

  1.   1
  2.   2
    1.     3
    2.     Why Flyback/buck Switching Is Noisy
    3.     Soft/quiet Fly-Buck Switching
    4.     Conclusion
    5.     Additional Resources

Eric Lee

My colleagues have written extensively about the Fly-Buck topology, but the details of the Fly-Buck’s soft/quiet switching characteristic haven’t been shared, which helps achieve higher efficiency, lower electromagnetic interference (EMI) and a smaller solution size in isolated DC/DC bias applications.

Why Flyback/buck Switching Is Noisy

In a flyback topology, the DC voltage stress across the switch is VIN + VOUT/N. On top of this DC voltage stress, high-frequency ringing caused by the transformer leakage inductance adds more stress at the moment the switch turns off; (Figure 1[a]). A resistor-capacitor-diode (RCD) snubber is usually required on the primary side to clamp and dampen ringing at the switching node (Figure 1[b]).

GUID-EAD9AEE4-2AEE-4D46-AC26-A3A0A624B21E-low.jpg Figure 1 Flyback Topology: Simplified Waveforms (a) and a Typical Flyback Circuit (b)

It is also very common to minimize the high-frequency ringing at the switching node when designing a buck converter by using an RC snubber in parallel with the low-side switch, as shown in Figure 2(a). In a buck topology, the ringing happens at the moment when the high-side switch turns on, as shown in Figure 2(b). The printed circuit board (PCB) trace inductance and reverse-recovery characteristic of the low-side body diode both affect the amount of ringing.

GUID-84899FEE-D46A-4E5E-A13F-82BB0755C73A-low.jpg Figure 2 Buck Topology: a Typical Synchronous Buck Circuit (a) and Simplified Waveforms (b)

Soft/quiet Fly-Buck Switching

In a Fly-Buck topology, the low-side switch turns on softly because the low-side body diode conducts before the switch turns on. The energy stored in the transformer leakage inductance always has a path to flow out. The high-side switch switches quietly because the low-side body diode is reverse-biased before the high-side switch turns on. Because the low-side body diode is reverse-biased, there is no reverse-recovery current flow when the high-side switch turns on.

The DC voltage stress across the switch is VIN; see Figure 3(b). Because the Fly-Buck switching is soft/quiet, just a small margin is required on top of VIN. Figure 3 shows a typical Fly-Buck circuit and switching waveforms. In Figure 3, im is the magnetizing current, which is the combination of the primary current and secondary current reflected to the primary side.

GUID-7C48AF1F-AB0A-4E8D-8578-3295A1D660B5-low.jpg Figure 3 Typical Fly-Buck Circuit (a) and Switching Waveforms (b)

Figure 4 shows the equivalent circuits of four switching modes. The four modes are:

  • MODE0: t0-t1 (energy store). The converter stores energy in the transformer when the high-side switch turns on. The primary-side current rises linearly during this period, similar to how the inductor current rises linearly in a buck.
  • MODE1: t1-t2 (high-side off to low-side on dead time). When the high-side switch turns off, the primary-side current keeps flowing through the low-side body diode after fully discharging/charging the low- and high-side parasitic capacitors. The secondary-side current starts flowing since the secondary-side diode is forward-biased. The switch-node voltage becomes almost zero before t2, which allows the low-side switch to turn on softly.
  • MODE2: t2-t3 (energy transfer). In this period, the low-side switch turns on and the converter transfers the stored energy to the secondary side, similar to how the flyback transfers energy to the secondary side when its low-side switch turns off. Assuming no/light load at the primary-side output, the primary-side current flows in a positive direction initially, but changes its direction to negative at the end of this period.
  • MODE3: t3-t0 (low-side off to high-side on dead time). The primary-side current flows in a negative direction in this period. This current discharges/charges the high- and low-side parasitic capacitors and reverse-biases the low-side body diode. Since the low-side body diode is reverse-biased before the high-side switch turns on, the high-side switch can turn on quietly at t0, without any excessive high-frequency ringing caused by the reverse-recovery effect. The secondary-side current stops flowing in this period since the secondary-side diode is reverse-biased.
GUID-7381D6BF-3E39-43F5-94A9-4D2F6445A201-low.jpg Figure 4 Equivalent Circuit of Each Mode and Current Flows: MODE0, T0-T1 (a); MODE1, T1-T2 (Dead Time) (b); MODE2, T2-T3 (c); and MODE3, T3-T0 (Dead Time) (d)

Conclusion

The Fly-Buck converter switches more quietly than the flyback or the buck. This quiet switching characteristic can bring some benefits beyond the Fly-Buck’s simplicity and good cross-regulation performance, including lower EMI; smaller board size, since the snubber circuit at the primary switch node is no longer necessary; and higher efficiency, by saving snubber loss on the primary side.

Additional Resources