SSZTAG8 january 2017
I'm told that the optimum environment for the human body is somewhere between 21°C and 30°C degrees, so inside TI’s air-conditioned office – set year-round to a toasty 23°C – conditions are perfect to deliver optimum performance (at least, that’s what my boss tells me).
In wintertime in central Europe, however, temperatures can fall to –20°C or lower. Even with many layers of clothing, the human body does not operate well under these conditions: it can survive, but it does not achieve optimum performance.
The human body is not the only thing affected by its operating conditions. Integrated circuits also operate best within certain temperature and supply-voltage ranges. In this post, I’ll discuss the latter, and the related undervoltage lockout (UVLO) function. You can find more details in the application report, “Understanding Undervoltage Lockout in Power Devices.”
Many devices have a UVLO threshold below a couple of volts. To be honest, it’s impressive that devices do anything at such low supply voltages. If you don’t believe me, try designing an analog circuit that operates from 2V and see how you get on.
The challenges are even greater in power devices. When the supply voltage is low, perhaps you can turn a power MOSFET on and off, but you can’t do it very quickly. And typically, the MOSFET’s on-resistance will increase, because the supply voltage is too low to generate a high-enough gate-source voltage.
Some devices specify a recommended supply-voltage range as well as a UVLO threshold. The device achieves full performance only if its supply voltage is in this range. But what happens between the UVLO threshold and the recommended minimum supply voltage? Several of TI’s power devices still function in this range, but their performance is not specified. That means that buck converters still buck, boost converters still boost and buck-boost converters still buck, boost or buck-boost, but the output power available may be less than the maximum the device is capable of.
In mission-critical applications, UVLO thresholds are typically above the minimum recommended supply voltage – the device turns on only when it can achieve full performance. This approach leads to extremely robust system designs, but in general is not cost-effective for consumer products. It would be like driving a car that stopped working as soon as the fuel level got low (but not empty). It’s more useful to have the car still drivable – albeit with reduced performance – than to suddenly stop working altogether.
Figure 1 illustrates the operational state of a typical power device. You can see that:
Figure 1 Typical UVLO BehaviorNote that the rising and falling UVLO thresholds are different. That is because a well-designed UVLO function has hysteresis. Why? Well, not only do comparator circuits in general benefit from hysteresis, power devices by their very nature tend to pull significant current from the upstream power supply. And since there’s always some resistance between the power supply and the device it’s powering, the voltage that the UVLO comparator sees is always a bit less than the voltage of the upstream power supply (see Figure 2). When the voltage reaches the UVLO threshold, the device turns off and the current flowing into it drops instantaneously to almost zero, causing the voltage that the UVLO comparator sees to immediately increase (because when the input current drops, the voltage drop across the input resistance suddenly disappears).
Figure 2 Equivalent Circuit of a Typical Power Device with UVLO FunctionIf the hysteresis voltage is smaller than I×R, under certain conditions the power management IC (PMIC) can turn on and off a number of times before it finally turns off for good. At best, this looks ugly; at worst, it can cause system-level problems. Figure 3 and Figure 4 are scope plots illustrating this phenomenon.
Figure 3 Low-input Resistance Results in Regular Power-down Behavior
Figure 4 High-input Resistance Results in Irregular Power-down BehaviorThe next time you're designing an application circuit, take a moment to make sure that you understand how the UVLO function works. For example:
Learn more about buck-boost converters.