SSZT969 august 2017
Technology is constantly getting smarter and smarter, from self-adjusting thermostats to voice-triggered appliances to automated factories. All of these technologies depend on the reliability of the grid infrastructure to provide power. Utility control centers need to communicate with electrical substations quickly and reliably to monitor power flowing across the grid. One way to communicate information is through Ethernet redundancy protocols, which increase the likelihood that information will reach its destination when a disruption in the network occurs.
Two emerging protocols for grid infrastructures are High-Availability Seamless Redundancy (HSR) and Parallel Redundancy Protocol (PRP). When used along with the Precision Time Protocol (PTP), these redundancy protocols can time-stamp the data packets. Keeping track of time helps synchronize information across the network and calculate where an event has occurred by converting the elapsed time into a distance. In this post, I will take a brief look at these two redundancy protocols and how to implement them.
Figure 1 HSR Ring
Figure 2 PRP Star NetworkTI is working on full support for all RTOS features for the Linux version, as well as expanding Linux support to the AM335x and AM437x processors. For a more complete comparison between RTOS- and Linux-supported features, see the Processor SDK HSR PRP TI Wiki page.