Small-signal Analysis
According to the traditional small-signal analysis, there are two important parameters which affect the output undershoot: the loop response of the converter and the output impedance of the power stage. Table 2 shows the factors that optimize the loop response and output impedance.
Table 2 Factors That Improve the Loop Response and Lower the Output Impedance
| Key parameters |
Factors for performance improvement |
|
Fast loop response
|
- High crossover frequency.
- Fast switching.
- Low-value inductor/high right-half-plane (RHP) zero frequency.
|
|
Low output impedance
|
- High-value output capacitor.
- High crossover frequency.
|
Large-signal Analysis
In addition to the two parameters in small-signal analysis, three more parameters in large-signal analysis affect the output undershoot: the error amplifier to pulse-width modulator (PWM) comparator offset, the
error amplifier sourcing capability and the wake-up delay. Because all three parameters are device-dependent and none are user-adjustable or user-programmable, device selection is very important when designing a pre-boost converter.
Error Amplifier to PWM Comparator Offset
Traditional boost devices have about 1.2V offset from the error-amplifier output to the input of the PWM comparator (see Figure 1). Because the device cannot start switching until the error amplifier output is greater than the offset
voltage, minimizing this offset is a key factor to improve undershoot during the battery voltage drop.
Error Amplifier Sourcing Capability
Sometimes the undershoot increases due to the limitation of the error amplifier. Ideally, the gain of the error amplifier should be constant over the typical error amplifier operating range, but the gain drops if
the error amplifier sourcing capability is insufficient.
Wake-up Delay
Because a pre-boost converter usually falls into a low quiescent current (IQ) standby mode to minimize battery drain when the battery voltage is in normal range, it takes some time to wake up the device
from a low-IQ standby mode. Because the device cannot start switching until it wakes up, excessive undershoot can occur during a long wake-up delay.
LM5150-Q1 Automotive Boost Controller
The LM5150-Q1 is a 2.2MHz automotive boost controller that features ultra-low IQ in standby mode. Specifically designed for use in start-stop systems as a pre-boost converter, the device has only 0.3V
offset and a strong transconductance error amplifier. The wake-up delay is less than 6µs, which is among the fastest in the industry.
Figure 2 is a comparison between a traditional boost converter and the LM5150-Q1. While the
output undershoot using the traditional boost conversion is big and greatly affected by a long wake-up time, a large offset and an insufficient error amplifier sourcing capability, the output undershoot using the LM5150-Q1 is small and
minimized. The traditional boost converter’s parameters are set to 1.2V offset, with a 100µA source current limit, a 2mA/V transconductance error amplifier gain and a 50µs wake-up delay.
Conclusion
A pre-boost converter’s output undershoot is affected by device selection. The output undershoot using the LM5150-Q1 is minimized by its small offset, large error amplifier sourcing capability and a quick wake-up
time.