SPRZ423K October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
Figure 2-1 provides an example of the 2807x device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 2-1. Some prototype devices may have markings different from those illustrated. Figure 2-2 shows an example of the device nomenclature.
Figure 2-1 Example
of Package Symbolization – PTP| SILICON REVISION CODE | SILICON REVISION | REVID(1) Address: 0x5D00C |
COMMENTS |
|---|---|---|---|
| B | B | 0x0002 | This silicon revision is available as TMX. |
| C | C | 0x0003 | This silicon revision is available as TMS. |
Figure 2-2 Example
of Device Nomenclature