SPRUIV2 April   2020

 

  1.   C2000 Gen 2 to Gen 3 MCUs Functional Safety Enablers
    1.     Trademarks
    2. 1 Introduction
    3. 2 References

Introduction

Safety mechanisms play an important role in safe-ing sensing, processing, actuation, communications and infrastructure capabilities that could be susceptible to permanent and transient faults. Figure 2 shows some of the key safety mechanisms that are available on the latest C2000 Generation 3 MCUs.

fig2.pngFigure 2. Key Safety Mechanisms in the Latest C2000 Generation 3 MCUS

These safety mechanisms enable enhancing system safety capability without compromising the real-time-control latency requirements. Some of the key safety mechanisms featured on our generation 3 MCUs include:

  • Background-CRC (BGCRC): Allows CRC checking program code without using CPU MIPs
  • Embedded Real-time Analysis & Diagnostics (ERAD): can be used for advanced system level diagnostics
  • Configurable Logic Block (CLB): used for implementing complex system-level PWM protection schemes while also reducing overall system BOM costs

C2000 provides over 300 safety mechanisms to use in the development of functional safety-compliant systems up to the safety integrity levels of ASIL D and SIL 3 as defined by the ISO 26262 and IEC 61508 functional safety standards, respectively. This document outlines some of the new safety mechanisms that have been introduced in the latest C2000 Generation 3 MCUs that customers can take advantage of in the development of their next generation functional safety compliant systems. Table 1 outlines the capability supported in our Generation 2 MCUs and the new (more effective or more efficient) capabilities on our Generation 3 MCUs.

Table 1. New/Improved Safety Mechanisms in the Gen3 Devices

NO Safety Requirement Capability Supported by Gen2 Devices New Capability Supported by Gen3 Devices Description F2807x/
F2837xS/D
F28004x F28002x
1 Clock integrity check External clock monitoring or software based clock monitoring using Timer or HRPWM module Dual Clock Comparator (DCC) Dedicated hardware based clock monitor freeing up CPU MIPS and peripherals for application usage
2 CPU integrity check (CPU permanent fault detection) Customer developed test. No quantified structural coverage C2000™ Hardware Built-In Self-Test Patented technology to provide high diagnostic coverage in a very short duration
3 Real time analysis and diagnostics for the CPU No hardware support. Complex software based checks required Embedded Real Time Analysis and Diagnostics (ERAD) engine Dedicated hardware module to help with system analysis and diagnostics
4 Data integrity check, end to end (E2E) safeing Software based CRC computation Accelerators: Enhancing the Capabilities of the C2000 MCU Family Technical Brief Co-processor with new instructions to make CRC computations faster
5 Continuous independent monitor for the CPU. Support for diagnostic execution without impacting critical control loop execution No capability existed CLA background task CLA is enhanced with interruptible background task capability whereby the diagnostic (monitoring) software can be executed as a lower priority task without compromising the real time control performance
6 CLA integrity check (CLA permanent fault detection) Customer developed test. No quantified structural coverage C2000™ CLA Self-Test Library Developed to be used for both start-up and application time self-test
7 Interrupt vector memory integrity check Software based periodic checks PIE double SRAM hardware comparison Dual modular redundancy for interrupt vector memory
8 Flash integrity check No capability existed ECC Flash memory supports Single Error Correction, Double Error Detection (SECDED) Error Correcting Code (ECC) diagnostic with coverage for both address and data bits
9 SRAM and ROM integrity check No capability existed ECC or parity Selected on-chip SRAMs and ROMs support SECDED ECC or parity diagnostic with coverage for both address and data bits
10 SRAM and ROM integrity check at boot-up Software based boot-time checks C2000 Memory Power-On Self-Test (M-POST) Fast power-on self-test of memory using dedicated hardware
11 SRAM and ROM integrity check during application Software based periodic checks Background CRC Patented technology to perform CRC check of static memory content and scrubbing of dynamic memory contents without application MIPS consumption
12 CLA program ROM integrity check during application Software based periodic checks Background CRC for CLA program ROM Patented technology to perform CRC check of CLA program ROM in the background without application MIPS consumption.
13 Advanced PWM fault detection Fault detection using external components like CPLD or FPGA ePWM fault detection using CLB Configurable Logic Block (CLB) can be used for detecting different erroneous conditions (e.g. Wrong dead-band, incorrect waveform, and so forth) which the PWMs will generate in the presence of faults
14 ADC conversion plausibility check Software based checks ADC post processing block Additional hardware added to ADC module to perform plausibility check
15 ADC pin integrity check No capability existed Opens and shorts detection circuit for ADC input pin Built in diagnostics which can be executed during start-up or during application time to identify opens or shorts on the ADC pin
16 Comparator reference integrity check No capability existed VDAC conversion by ADC Correct functioning of comparator is very critical from a system safety perspective. The reference voltage of the comparator can be checked using this.
17 Reliable high-speed communication across isolation barriers Serial Peripheral Interface Fast Serial Interface (FSI) Several built in diagnostics (e.g. hardware ping to detect line breaks, data ECC, CRC, and so forth.) and hardware features (skew compensation, Double Data Rate (DDR), and so forth.) to support high speed reliable communication
18 Watchdog with separate time base and time-window Watchdog with separate time base Windowed watchdog Windowed watchdog with counter running on an independent clock
19 Prevention of unintended register programmation due to faults Periodic software read-back of register Multi-bit enable keys for control registers Prevents unintentional activation/deactivation as multiple bits need to be correct to enable or disable the critical functionality.
20 Prevention of unintended register programmation due to faults Periodic software read-back of registers Lock mechanism for registers Write access to the registers can be blocked or enabled by configuring the lock bits
21 Critical error intimation to external world GPIO based critical error intimation using software ERRORSTS pin Dedicated (configurable pin) to intimate critical errors to external world without software intervention
22 Freedom from interference - avoid interference from unused modules Software intensive check Peripheral soft reset This capability can be used to keep the unused peripherals in reset.
23 Freedom from interference - access (e.g. fetch, write) gating for individual RAM blocks from different masters (viz. CPU,CLA,DMA) No capability existed Access protection mechanism for memories This configuration can be changed during run-time and allows memory to block access from specific masters or specific application threads within the same master
24 Freedom from interference – access gating for individual peripherals from different masters No capability existed Peripheral access protection This configuration can be changed during run-time and allows peripherals to block access from specific masters or specific application threads within the same master
25 Freedom from interference - ability to run two independent application threads without interference No capability existed except for F2805x Achieving Coexistence of Safety Functions for EV/HEV Using C2000 MCUs Application threads with different safety integrity levels can be executed from different security zones (for example, zone1, zone2.) thus mitigating the risk due to interference from one function to another

Detailed descriptions for each of the above mentioned safety mechanisms can be found in the Functional Safety Manual for the corresponding C2000 Generation 3 MCUs. For a list of Functional Safety related collateral for C2000 including Functional Safety Manuals, Diagnostic Software Library, compiler qualification kits, third party operating systems and development tools and additional Functional Safety related documentation, see the C2000 Functional Safety Enablers. To learn more about C2000 Functional Safety, see http://www.ti.com/microcontrollers/c2000-real-time-control-mcus/overview.html#safety.