SPRUIG8I January 2018 – December 2023
You can inspect or modify
library functions by examining the source code in
the lib/src subdirectory of the compiler
installation. For example,
C:\ti\ccsv7\tools\compiler\c7000_#.#.#\lib\src
.
One you have located the relevant source code, change the specific function file and rebuild the library.
You can use this source tree to rebuild the rts7100_le.lib, rts7100_le_eh.lib, rts7100_be.lib, or rts7100_be_eh.lib library or to build a new library. See Section 7.1.8 for details on library naming and Section 7.4 for details on building