SNOA952 May   2016 FDC2112 , FDC2112-Q1 , FDC2114 , FDC2114-Q1 , FDC2212 , FDC2212-Q1 , FDC2214 , FDC2214-Q1

 

  1.   Ground Shifting in Capacitive Sensing Applications
    1.     Trademarks
    2. 1 Introduction
    3. 2 Mathematical Modeling
      1. 2.1 Different Grounding Configurations
        1. 2.1.1 Earth Ground Referenced
        2. 2.1.2 Floating Ground Referenced
          1. 2.1.2.1 Large Local Ground Plane
    4. 3 Qualitative Test Setup
      1. 3.1 Earth Ground Referenced Laptop
      2. 3.2 Floating Laptop
      3. 3.3 Floating Laptop With Large Local Ground Plane
    5. 4 Conclusion

Large Local Ground Plane

A way of compensating for this ground shift is to increase Cg by introducing a large local ground plane. The ground plane needs to be large in order to increase the effective Cg. Figure 3 shows the system configuration when the laptop is floating and battery-powered but there is a large ground plane that is connected to the local ground of the FDC2214 EVM through a short wire where:

  • Cpg is the fixed parasitic capacitance between the large local ground plane and earth ground
  • Cp0 is the fixed parasitic capacitance introduced by the large local ground plane
FloatingwithGNDPlate.gifFigure 3. Simplified Model of the FDC2214 EVM Board Floating With a Large Local Ground Plane Nearby

In this configuration, Cpg and Cg are in parallel which effectively increases the overall capacitance between local and earth ground. Because Cg effectively increases, β also increases closer to 1 which helps mitigate the ground shift effect.

NOTE

Cp0 and C0 are also in parallel which effectively increases the resonator’s total capacitance.

Due to this increased capacitance, the signal seen at Cs will become diluted and the sensitivity of the system will decrease. However, this also means that the observed ground shift effect is slightly minimized:

Equation 9. equation_04_snoa952.gif
Equation 10. equation_02_snoa952.gif
Equation 11. equation_06_snoa952.gif

For example, if CP0 is 10 times larger than C0, then the oscillation frequency equation becomes as follows

Equation 12. equation_11_snoa952.gif

where changes in βCs, the series combination of (Cg| |Cpg) and Cs, will have less of an effect on the oscillation frequency than if there was no large nearby ground plane. However, this is more of a second-order effect – the ground shift phenomenon is more directly dependent on how large the effective Cg is.