SNLU271B March 2020 – June 2022
Download the software from https://www.ti.com/tool/usb-2-mdio .
The web page also contains the User’s Guide for installing and using the software. Since the MSP430 is on-board the DP83TD510E-EVM, it is not necessary to purchase a separate MSP430 Launchpad kit and connect to the PHY using wires. In the case the on-board MSP430 cannot be used for some reason, MDIO and MDC pins are also broken out on J23 and J22 pins, respectively. Users can connect an MSP430 launchpad or their own MDIO-MDC utility on J23 and J22 to access the PHY.