SNLA419 October 2022 TDP1204 , TMDS1204
The TMDS1204 and TDP1204 are HDMI 2.1 redrivers that support AEQ functionality that provides a cost-effective solution to applications that have dynamic channel characteristics. The procedure to use the AEQ functionality for both devices was given by using the example of the TMDS1204 EVM. This procedure can help to provide direction to other design when integrating the TMDS1204 or TDP1204 into other applications. Lastly, this document provided test results following the test procedure to show that AEQ functionality can correctly select the right EQ value to equalize the channel.