SNAU283 October   2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Evaluation Board Kit Contents
  4. 2Quick Start
    1. 2.1 Quick Start Description
      1. 2.1.1 Clock Outputs Page Description
      2. 2.1.2 TICS Pro Tips
  5. 3PLL Loop Filters and Loop Parameters
    1. 3.1 PLL1 Loop Filter
    2. 3.2 PLL2 Loop Filter
  6. 4Default TICS Pro Mode
  7. 5Using TICS Pro to Program the LMK04368-EP
    1. 5.1 Start TICS Pro Application
    2. 5.2 Select Device
    3. 5.3 Program the Device
    4. 5.4 Restoring a Default Mode
    5. 5.5 Visual Confirmation of Frequency Lock
    6. 5.6 Enable Clock Outputs
  8. 6Evaluation Board Inputs and Outputs
  9. 7Recommended Test Equipment
  10. 8Schematics
  11. 9Bill of Materials
  12.   A USB2ANY Firmware Upgrade
  13.   B TICS Pro Usage
    1. 11.1  Communication Setup
    2. 11.2  User Controls
    3. 11.3  Raw Registers Page
    4. 11.4  Set Modes Page
    5. 11.5  Holdover Page
    6. 11.6  CLKinX Control Page
    7. 11.7  PLL1 and 2 Page
    8. 11.8  SYNC / SYSREF Page
    9. 11.9  Clock Outputs Page
    10. 11.10 Other Page
    11. 11.11 Burst Mode Page

USB2ANY Firmware Upgrade

When the onboard USB2ANY programmer is first connected, or if the firmware revision used for the onboard USB2ANY programmer does not match the version used by TICS Pro (2.7.0.0), TICS Pro will request a firmware update. Follow the pop-up instructions to complete the update.

  1. When the USB2ANY Firmware Requirement pop-up window appears, click OK to continue.
    GUID-5CD613ED-3018-4F72-AA55-DE57A7884B48-low.png Figure A-1 Firmware Requirement
  2. The Firmware Loader pop-up window will load. Disconnect the USB cable from the EVM.
    GUID-C2A6F933-3EFC-4959-9D8E-35483FBAEC5A-low.png Figure A-2 Firmware Loader
  3. Press and hold the BSL button while you connect the USB2ANY cable.
    GUID-AA6C6B43-69E0-4127-89DC-56812C9F8F8F-low.png Figure A-3 BSL Button Location
  4. The firmware loader should recognize the USB2ANY as a target for programming, and an Update Firmware button should appear.
    GUID-BB1EB6A7-67B7-4FD0-A911-FBFB0887EB69-low.png Figure A-4 Update Firmware
  5. Click Upgrade Firmware to start the firmware upgrade. Click Close after the upgrade is complete.
    GUID-B7936C82-4846-434C-A0B8-8EE566DE6D64-low.png Figure A-5 Firmware Update Complete
  6. Go to USB communications → Interface in the TICS Pro software to check the USB connection. Make sure the USB Connected button is green.
    GUID-08F4612E-57AE-4418-855A-812FC26E13E6-low.png Figure A-6 USB Communications