SLVUAW9C September   2016  â€“ February 2020 UCD90320

 

  1.   UCD90320 Sequencer and System Health Controller PMBus Command Reference
    1.     Trademarks
    2. 1  PMBus Specification
      1. 1.1 Manufacturer Specific Status (STATUS_MFR_SPECIFIC)
    3. 2  Data Formats
      1. 2.1 Data Format for Output Voltage Parameters
      2. 2.2 Data Format for Other Parameters
      3. 2.3 Distinguishing Between Linear Data Formats
      4. 2.4 Translation, Quantization, and Truncation
      5. 2.5 8-Bit Time Encoding
    4. 3  Memory Model
    5. 4  Alert Response Address Support
    6. 5  Supported PMBus Commands
    7. 6  Implementation Details for PMBus Core Commands
      1. 6.1  (00h) PAGE
      2. 6.2  (01h) OPERATION
      3. 6.3  (11h) STORE_DEFAULT_ALL
      4. 6.4  (12h) RESTORE_DEFAULT_ALL
      5. 6.5  (1Bh) SMBALERT_MASK
      6. 6.6  (20h) VOUT_MODE
      7. 6.7  (38h) IOUT_CAL_GAIN
      8. 6.8  (41h – 69h) xxx_FAULT_RESPONSE
      9. 6.9  (62h) TON_MAX_FAULT_LIMIT
      10. 6.10 (66h) TOFF_MAX_WARN_LIMIT
      11. 6.11 (80h) STATUS_MFR_SPECIFIC
      12. 6.12 (81h) STATUS_FAN_1_2 and (82h) STATUS_FAN_3_4
      13. 6.13 (8Dh) READ_TEMPERATURE_1
      14. 6.14 (8Eh) READ_TEMPERATURE_2
      15. 6.15 (90-93h) FAN_SPEED_1 Through FAN_SPEED_4
      16. 6.16 (ADh) IC_DEVICE_ID
      17. 6.17 (AEh) IC_DEVICE_REV
    8. 7  Input and Output Pin Configuration
    9. 8  PWM Configuration
    10. 9  Implementation Details for User Data Commands
      1. 9.1 (B5h) BLACK_BOX_FAULT_INFO (USER_DATA_05)
        1. 9.1.1 Fault Info
      2. 9.2 (B6h) BLACK_BOX_FAULT_RAILS_WARNING(USER_DATA_06)
      3. 9.3 (B7h) BLACK_BOX_LOG_RAILS_VALUE(USER_DATA_07)
      4. 9.4 (B8h) RAIL_PROFILE(USER_DATA_08)
        1. 9.4.1 Number Profile
        2. 9.4.2 Profile Index
      5. 9.5 (B9h) RAIL_STATE (USER_DATA_09)
    11. 10 Implementation Details for Manufacturer-Specific Commands
      1. 10.1  (D0h) FAULT_PIN_CONFIG (MFR_SPECIFIC_00)
        1. 10.1.1 Fault Pin Configuration
        2. 10.1.2 Page Mask
        3. 10.1.3 Other Mask
      2. 10.2  (D1h) VOUT_CAL_MONITOR (MFR_SPECIFIC_01)
      3. 10.3  (D2h) SYSTEM_RESET_CONFIG (MFR_SPECIFIC_02)
        1. 10.3.1 GPI Flags
        2. 10.3.2 Page Flags
        3. 10.3.3 De-Assert When Power-Good
        4. 10.3.4 Assert When NOT Power-Good
        5. 10.3.5 Assert When Watchdog Timeout
        6. 10.3.6 Delay Time
        7. 10.3.7 Pulse Time
        8. 10.3.8 GPI Tracking
        9. 10.3.9 Reset Pin Configuration
      4. 10.4  (D3h) SYSTEM_WATCHDOG_CONFIG (MFR_SPECIFIC_03)
        1. 10.4.1 Enable
        2. 10.4.2 Watch System Reset Pin
        3. 10.4.3 Max Fan Speed With Timeout
        4. 10.4.4 Disable Until System Reset Release
        5. 10.4.5 Start Time
        6. 10.4.6 Input Pin (WDI) Configuration
        7. 10.4.7 Reset Period
        8. 10.4.8 Output Pin (WDO) Configuration
      5. 10.5  (D4h) SYSTEM_WATCHDOG_RESET (MFR_SPECIFIC_04)
      6. 10.6  (D5h) MONITOR_CONFIG (MFR_SPECIFIC_05)
      7. 10.7  (D6h) NUM_PAGES (MFR_SPECIFIC_06)
      8. 10.8  (D7h) RUN_TIME_CLOCK (MFR_SPECIFIC_07)
      9. 10.9  (D8h) RUN_TIME_CLOCK_TRIM (MFR_SPECIFIC_08)
      10. 10.10 (D9h) ROM_MODE (MFR_SPECIFIC_09)
      11. 10.11 (DAh) USER_RAM_00 (MFR_SPECIFIC_10)
      12. 10.12 (DBh) SOFT_RESET (MFR_SPECIFIC_11)
      13. 10.13 (DCh) RESET_COUNT (MFR_SPECIFIC_12)
      14. 10.14 (DDh) PIN_SELECTED_RAIL_STATES (MFR_SPECIFIC_13)
        1. 10.14.1 System State Enables
        2. 10.14.2 Soft-Off Enables
        3. 10.14.3 System State
      15. 10.15 (DEh) RESEQUENCE (MFR_SPECIFIC_14)
      16. 10.16 (DFh) CONSTANTS (MFR_SPECIFIC_15)
      17. 10.17 (E0h) PWM_SELECT (MFR_SPECIFIC_16)
      18. 10.18 (E1h) PWM_CONFIG (MFR_SPECIFIC_17)
      19. 10.19 (E2h) PARM_INFO (MFR_SPECIFIC_18)
      20. 10.20 (E3h) PARM_VALUE (MFR_SPECIFIC_19)
      21. 10.21 (E4h) TEMPERATURE_CAL_GAIN (MFR_SPECIFIC_20)
      22. 10.22 (E5h) TEMPERATURE_CAL_OFFSET (MFR_SPECIFIC_21)
      23. 10.23 (E9h) FAULT_RESPONSES (MFR_SPECIFIC_25)
        1. 10.23.1 Fault Response Bytes
        2. 10.23.2 Resequence
        3. 10.23.3 Time Between Retries
        4. 10.23.4 Maximum Glitch Time for Voltage Faults
        5. 10.23.5 Maximum Glitch Time for Non-Voltage Faults
      24. 10.24 (EAh) LOGGED_FAULTS (MFR_SPECIFIC_26)
        1. 10.24.1 Command Format
        2. 10.24.2 Non-Paged Faults
        3. 10.24.3 GPI Faults
        4. 10.24.4 Page-Dependent Faults
      25. 10.25 (EBh) LOGGED_FAULT_DETAIL_INDEX (MFR_SPECIFIC_27)
      26. 10.26 (ECh) LOGGED_FAULT_DETAIL (MFR_SPECIFIC_28)
      27. 10.27 (EDh) LOGGED_PAGE_PEAKS (MFR_SPECIFIC_29)
      28. 10.28 (EEh) LOGGED_COMMON_PEAKS (MFR_SPECIFIC_30)
      29. 10.29 (EFh) LOGGED_FAULT_DETAIL_ENABLES (MFR_SPECIFIC_31)
      30. 10.30 (F0h) EXECUTE_FLASH (MFR_SPECIFIC_32)
      31. 10.31 (F1h) SECURITY (MFR_SPECIFIC_33)
        1. 10.31.1 Enabling Security
        2. 10.31.2 Disabling Security
        3. 10.31.3 Reading This Command
      32. 10.32 (F2h) SECURITY_BIT_MASK (MFR_SPECIFIC_34)
      33. 10.33 (F3h) MFR_STATUS (MFR_SPECIFIC_35)
      34. 10.34 (F4h) GPI_FAULT_RESPONSES (MFR_SPECIFIC_36)
        1. 10.34.1 Fault Responses Byte
        2. 10.34.2 Time Between Retries
        3. 10.34.3 Max Glitch Time for GPI
        4. 10.34.4 GPI Number Rail Profile Pin Selection
        5. 10.34.5 Block Out Period for Profile
      35. 10.35 (F5h) MARGIN_CONFIG (MFR_SPECIFIC_37)
      36. 10.36 (F6h) SEQ_CONFIG (MFR_SPECIFIC_38)
        1. 10.36.1  Enable Pin Configuration
        2. 10.36.2  GPI Sequence On Dependency Mask
        3. 10.36.3  GPI Sequence Off Dependency Mask
        4. 10.36.4  Sequencing Timeout Configuration
        5. 10.36.5  Sequencing On Timeout
        6. 10.36.6  Sequencing Off Timeout
        7. 10.36.7  Page Sequence On Dependency Mask
        8. 10.36.8  Page Sequence Off Dependency Mask
        9. 10.36.9  Fault Slaves Mask
        10. 10.36.10 GPO Sequence On Sependency Mask
        11. 10.36.11 GPO Sequence Off Sependency Mask
      37. 10.37 (F7h) GPO_CONFIG_INDEX (MFR_SPECIFIC_39)
      38. 10.38 (F8h) GPO_CONFIG (MFR_SPECIFIC_40)
        1. 10.38.1  Output Pin Configuration
        2. 10.38.2  Assert Delay Enable
        3. 10.38.3  De-Assert Delay Enable
        4. 10.38.4  Invert OR Output
        5. 10.38.5  Ignore Inputs During Delay
        6. 10.38.6  Invert AND Output
        7. 10.38.7  State Machine Mode Enable
        8. 10.38.8  High Resolution Delay Count
        9. 10.38.9  9 Millisecond Delay
        10. 10.38.10 Status Mask
        11. 10.38.11 Status Inversion Mask
        12. 10.38.12 GPI Mask
        13. 10.38.13 GPI Inversion Mask
        14. 10.38.14 GPO Mask
        15. 10.38.15 GPO Inversion Mask
        16. 10.38.16 Status Type Select
        17. 10.38.17 GPO Configuration Examples
      39. 10.39 (F9h) GPI_CONFIG (MFR_SPECIFIC_41)
        1. 10.39.1 GPI Pin Configuration
          1.        Table 1. Fault Enable Bits
        2. 10.39.2 Sequence Timeout Pin Selection
        3. 10.39.3 Latched Statuses Clear Pin Selection
        4. 10.39.4 MRG_EN Pin Selection
        5. 10.39.5 MRG_LOW_nHIGH Pin Selection
        6. 10.39.6 Debug Mode Pin Selection
      40. 10.40 (FAh) GPIO_SELECT (MFR_SPECIFIC_42)
      41. 10.41 (FBh) GPIO_CONFIG (MFR_SPECIFIC_43)
      42. 10.42 (FCh) MISC_CONFIG (MFR_SPECIFIC_44)
        1. 10.42.1 Miscellaneous Configuration Byte
        2. 10.42.2 Time Between Resequences
        3. 10.42.3 External Reference Voltage
        4. 10.42.4 Resequence_rails_mask
      43. 10.43 (FDh) DEVICE_ID (MFR_SPECIFIC_45)
    12. 11 Range Checking and Limits
    13. 12 Glossary

(F6h) SEQ_CONFIG (MFR_SPECIFIC_38)

This Read/Write Block command configures the sequencing dependencies and enable pin for a given rail.

Features include:

  • Sequencing – Configures interdependency between how voltage rails are enabled/disabled
  • Fault Slaves – Configure slave pages which also shut down when a fault occurs
  • Enable Pin – Identifies the enable pin, and its operating characteristics.

NOTE

All configurations done with the GPI_CONFIG command must be done before writing this command.

NOTE

When this command is written, the enable pin for the rail is de-asserted. Then the state of the rail is reevaluated. If it is determined that the rail should be on, the enable pin is asserted.

Table 59. SEQ_CONFIG Command Format

Byte Number
(Write)
Byte Number
(Read)
Payload
Index
Description
0 CMD = F6
1 0 BYTE_COUNT = 29
2 1 0 Enable Pin Configuration
it Definitions:
7:0: Pin Id of Enable Pin
3 2 1 Enable Pin Configuration
Bit Definitions:
7:3: Reserved
2: Polarity of Enable pin
1:0 Pin Mode of Enable Pin
4 3 2 GPI Sequence On Dependency Mask (Byte 0 - LSB)
5 4 3 GPI Sequence On Dependency Mask (Byte 1)
6 5 4 GPI Sequence On Dependency Mask (Byte 2)
7 6 5 GPI Sequence On Dependency Mask (Byte 3 - MSB)
8 7 6 GPI Sequence Off Dependency Mask (Byte 0 - LSB)
9 8 7 GPI Sequence Off Dependency Mask (Byte 1)
10 9 8 GPI Sequence Off Dependency Mask (Byte 2)
11 10 9 GPI Sequence On Dependency Mask (Byte 3 - MSB)
12 11 10 Sequencing Timeout Configuration
13 12 11 Sequencing On Timeout
14 13 12 Sequencing Off Timeout
15 14 13 Page Sequence On Dependency Mask (Byte 0 - LSB)
16 15 14 Page Sequence On Dependency Mask (Byte 1)
17 16 15 Page Sequence On Dependency Mask (Byte 2)
18 17 16 Page Sequence On Dependency Mask (Byte 3 - MSB)
19 18 17 Page Sequence Off Dependency Mask (Byte 0 - LSB)
20 19 18 Page Sequence Off Dependency Mask (Byte 1)
21 20 19 Page Sequence Off Dependency Mask (Byte 2)
22 21 20 Page Sequence Off Dependency Mask (Byte 3 - MSB)
23 22 21 Fault Slaves Mask (Byte 0 - LSB)
24 23 22 Fault Slaves Mask (Byte 1)
25 24 23 Fault Slaves Mask (Byte 2)
26 25 24 Fault Slaves Mask (Byte 3 - MSB)
27 26 25 GPO Sequence Off Dependency Mask(Byte 0 – LSB)
28 27 26 GPO Sequence On Dependency Mask(Byte 1)
29 28 27 GPO Sequence Off Dependency Mask(Byte 0 – LSB)
30 29 28 GPO Sequence Off Dependency Mask(Byte 1)

The turn on condition for each page can depend on the state of several other pages and/or input pins. The same pages and pins also may be used to control multiple pages. The GPI and Page dependencies (Sequence On Dependencies) define a set of conditions which allow a page to turn on when met. Note that the logical AND of all conditions must be met. Once the page is on, these dependencies have no further effect on the operating status of the page. Specifically, they do not cause a page to turn off.

Sequence On Dependencies work in parallel with the PMBus defined mechanisms used to enable an output. That is, both the Sequence On Dependencies and the PMBus mechanism must be satisfied. For example, if the page responds to an OPERATION command, until ON is specified by the command, the page remains off even if all of the sequencing Sequence On Dependencies are met. Further, the order in which they are met is irrelevant; the OPERATION command can be issued first and then the sequencing requirements, when met, turn on the output, or the sequencing requirements can be met first in which case the page would wait for the command. In the ON_OFF_CONFIG command a “None” setting, is still subject to the specified Sequence On Dependencies.

Turn on delay (TON_DELAY) is applied after the page has been commanded on and Sequence On Dependencies are met.

Unless the rail is instructed to turn off immediately, these same comments apply to the Sequence Off Dependencies – they must be met before the rail is turned off, the turn off delay (TOFF_DELAY) is applied after the dependencies are met, etc.

After a fault, the PMBus specification declares that an OFF/ON sequence occur before the rail is allowed to restart. Note that the toggle of sequencing pin is interpreted to meet this requirement. For example, consider a page that responds to the CTRL_PIN and has a Turn-On Dependency which shuts down due to a fault. A toggle low then high on either the CTRL_PIN or the sequencing pin is sufficient to restart the page.

NOTE

Some tables in the following subsections assume that the device supports 16 rails (0 to 15). For a given device, this may not be the case. The interpretation of this information should be adjusted for the correct number of rails.