SLVSC31D December 2013 – August 2015
PRODUCTION DATA.
Figure 28. Example of Layout
Figure 29. Typical HKU Package With Leads Form
Figure 30. Typical Thermal Vias Footprint
Figure 31. Typical Thermal Vias Details
The power-handling capability of the device is limited by the maximum-rated junction temperature (125°C). The power dissipated by the device is made up of two components:
Find the GND pin current by using the GND pin current graphs in Typical Characteristics. Power dissipation is equal to the sum of the two components listed previously.
The TPS7A4501-SP regulators have internal thermal limiting designed to protect the device during overload conditions. For continuous normal conditions, do not exceed the maximum junction temperature rating of 125°C. It is important to give careful consideration to all sources of thermal resistance from junction to ambient. Also consider additional heat sources mounted nearby.
For surface-mount devices, heat sinking is accomplished by using the heat-spreading capabilities of the PCB and its copper traces. Copper board stiffeners and plated through-holes can also be used to spread the heat generated by power devices.
Example: Given an output voltage of 3.3 V, an input voltage range of 4 to 6 V, an output current range of 0 to 500 mA, and a maximum case temperature of 50°C, what is the maximum junction temperature?
The power dissipated by the device is equal to:
where
So,
Using a U package, the thermal resistance is about 10.3°C/W. So the junction temperature rise above case is approximately equal to:
The maximum junction temperature is then equal to the maximum junction-temperature rise above case plus the maximum case temperature or: