SLVS941G April 2009 – August 2016 TPS62230
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS6223x device family are high-frequency, synchronous, step-down DC-DC converters providing switch frequencies up to 3.8 MHz. Different fixed output voltage versions are available from 1.0 V to 3.3 V.
Figure 5. TPS62230 2.5-V Output
The device operates over an input voltage range from 2.05 V to 6 V. The device family offers a broad range of internally fixed output voltage options from 1 V to 3.3 V. The TPS6223x is easy to use and needs just three external components; however, the selection of external components and PCB layout must comply with the design guidelines to achieve specified performance.
The TPS6223x is optimized to operate with effective inductance values in the range of 0.7 μH to 4.3 μH and with effective output capacitance in the range of 2.0 μF to 15 μF. The internal compensation is optimized to operate with an output filter of L = 1.0 μH/2.2 μH and COUT = 4.7 μF. Larger or smaller inductor/capacitor values can be used to optimize the performance of the device for specific operation conditions. For more details, see the Checking Loop Stability section.
The inductor value affects its peak-to-peak ripple current, the PWM-to-PFM transition point, the output voltage ripple and the efficiency. The selected inductor has to be rated for its DC resistance and saturation current. The inductor ripple current (ΔIL) decreases with higher inductance and increases with higher VIN or VOUT . Equation 5 calculates the maximum inductor current under static load conditions. The saturation current of the inductor must be rated higher than the maximum inductor current as calculated with Equation 6. This is recommended because during heavy load transient the inductor current will rise above the calculated value.
where
In high-frequency converter applications, the efficiency is essentially affected by the inductor AC resistance (that is, quality factor) and to a smaller extent by the inductor DCR value. To achieve high-efficiency operation, take care in selecting inductors featuring a quality factor above 25 at the switching frequency. Increasing the inductor value produces lower RMS currents, but degrades transient response. For a given physical inductor size, increased inductance usually results in an inductor with lower saturation current.
The total losses of the coil consist of both the losses in the DC resistance, R(DC), and the following frequency-dependent components:
The following inductor series from different suppliers have been used with the TPS6223x converters.
| INDUCTANCE (μH) |
DIMENSIONS (mm3) |
INDUCTOR TYPE | SUPPLIER(1) |
|---|---|---|---|
| 1.0 / 2.2 | 2.5 × 2.0 × 1.2 | LQM2HPN1R0MJ0 | Murata |
| 2.2 | 2.0 × 1.2 × 0.55 | LQM21PN2R2 | Murata |
| 1.0 / 2.2 | 2.0 × 1.2 × 1.0 | MIPSZ2012 | FDK |
| 1.0 / 2.2 | 2.0 × 2.5 × 1.2 | MIPSA2520 | FDK |
| 1.0 / 2.2 | 2.0 × 1.2 × 1.0 | KSLI2012 series | Hitachi Metal |
The unique hysteretic PWM control scheme of the TPS62230 allows the use of tiny ceramic capacitors. Ceramic capacitors with low ESR values have the lowest output voltage ripple and are recommended. The output capacitor requires either an X7R or X5R dielectric. Y5V and Z5U dielectric capacitors, aside from their wide variation in capacitance over temperature, become resistive at high frequencies.
At light load currents, the converter operate in power save mode and the output voltage ripple is dependent on the output capacitor value and the PFM peak inductor current. Higher output capacitor values minimize the voltage ripple in PFM mode and tighten DC output accuracy in PFM mode.
Because of the nature of the buck converter having a pulsating input current, a low-ESR input capacitor is required for best input voltage filtering and minimizing the interference with other circuits caused by high input voltage spikes. For most applications a 2.2-μF to 4.7-μF ceramic capacitor is recommended. The input capacitor can be increased without any limit for better input voltage filtering. Because ceramic capacitor loses up to 80% of its initial capacitance at 5 V, TI recommends using 4.7 μF input capacitors for input voltages > 4.5 V.
Take care when using only small ceramic input capacitors. When a ceramic capacitor is used at the input and the power is being supplied through long wires, such as from a wall adapter, a load step at the output or VIN step on the input can induce ringing at the VIN pin. This ringing can couple to the output and be mistaken as loop instability or could even damage the part by exceeding the maximum ratings.
Table 2 shows a list of tested input and output capacitors.
| CAPACITANCE [μF] | SIZE | CAPACITOR TYPE | SUPPLIER(1) |
|---|---|---|---|
| 2.2 | 0402 | GRM155R60J225 | Murata |
| 4.7 | 0402 | AMK105BJ475MV | Taiyo Yuden |
| 4.7 | 0402 | GRM155R60J475 | Murata |
| 4.7 | 0402 | CL05A475MQ5NRNC | Samsung |
| 4.7 | 0603 | GRM188R60J475 | Murata |
The first step of circuit and stability evaluation is to look from a steady-state perspective at the following signals:
These are the basic signals that need to be measured when evaluating a switching converter. When the switching waveform shows large duty cycle jitter or the output voltage or inductor current shows oscillations, the regulation loop may be unstable. This is often a result of board layout and/or L-C combination.
As a next step in the evaluation of the regulation loop, the load transient response is tested. The time between the application of the load transient and the turn on of the P-channel MOSFET, the output capacitor must supply all of the current required by the load. VOUT immediately shifts by an amount equal to ΔI(LOAD) x ESR, where ESR is the effective series resistance of COUT. ΔI(LOAD) begins to charge or discharge CO generating a feedback error signal used by the regulator to return VOUT to its steady-state value. The results are most easily interpreted when the device operates in PWM mode.
During this recovery time, VOUT can be monitored for settling time, overshoot or ringing that helps judge the converter’s stability. Without any ringing, the loop has usually more than 45° of phase margin.
Because the damping factor of the circuitry is directly related to several resistive parameters (for example, MOSFET rDS(on)) that are temperature dependant, the loop stability analysis has to be done over the input voltage range, load current range, and temperature range.
Figure 8. Efficiency PFM / PWM Mode, 1.2-V Output Voltage – TPS62232
Figure 10. Efficiency vs IOUT, PFM / PWM Mode – TPS62235
Figure 12. 1.2-V Output Voltage Accuracy PFM/PWM Mode – TPS62232
Figure 14. Switching Frequency vs Output Current, 1.2-V Output Voltage, Forced PWM Mode – TPS62232
Figure 9. Efficiency Forced PWM Mode, 1.2-V Output Voltage – TPS62232
Figure 11. 1.2-V Output Voltage Accuracy Forced PWM Mode – TPS62232
Figure 13. Switching Frequency vs Output Current, 1.2-V Output Voltage, PFM/PWM Mode – TPS62232
Figure 16. Efficiency PFM/PWM Mode, 1.8-V Output Voltage – TPS62231
Figure 18. Comparison Efficiency vs Inductor Value and Size – TPS62231
Figure 20. 1.8-V Output Voltage Accuracy Forced PWM Mode – TPS62231
Figure 22. Switching Frequency vs Output Current, 1.8-V Output Voltage, PFM/PWM Mode – TPS62231
Figure 17. Efficiency Forced PWM Mode, 1.8-V Output Voltage – TPS62231
Figure 19. 1.8-V Output Voltage Accuracy PFM / PWM Mode – TPS62231
Figure 21. Switching Frequency vs Output Current, 1.8-V Output Voltage, PFM/PWM Mode – TPS62231
Figure 23. Switching Frequency vs Output Current, 1.8-V Output Voltage, Forced PWM Mode – TPS62231
Figure 26. Efficiency PFM/PWM Mode, 2.5-V Output Voltage – TPS62230
Figure 28. 2.5V Output Voltage Accuracy Forced PWM Mode – TPS62230
Figure 30. Switching Frequency vs Output Current, 2.5-V Output Voltage, PFM/PWM Mode – TPS62230
Figure 27. Efficiency Forced PWM Mode, 2.5-V Output Voltage – TPS62230
Figure 29. 2.5-V Output Voltage Accuracy PFM/PWM Mode – TPS62230
Figure 31. Switching Frequency vs Output Current, 2.5-V Output Voltage, Forced PWM Mode – TPS62230
Figure 33. Start-Up in 1-V Prebiased Output – TPS62231
Figure 34. Start-Up into 20 Ω Load, VOUT 2.5 V – TPS62230
Figure 35. PFM Mode Operation, L = 1.0 µH,
Figure 37. Forced PWM Mode Operation IOUT = 10 mA – TPS62230
Figure 36. PFM Mode Operation, L = 2.2 µH,
Figure 38. Output Voltage, Peak-to-Peak vs Output Current – TPS62231
Figure 39. Output Voltage, Peak-to-Peak vs Output Current – TPS62230
Figure 40. 1.8-V Power-Supply Rejection Ratio – TPS62231
Figure 43. Line Transient Response, PFM Mode – TPS62231
Figure 44. Line Transient Response, PWM Mode – TPS62231
Figure 45. Mode Transition PFM / Forced PWM Mode – TPS62231
Figure 46. AC – Load Regulation Performance 1.8-V VOUT, PFM Mode – TPS62231
Figure 48. AC – Load Regulation Performance 2.5-V VOUT, PWM Mode – TPS62230
Figure 47. AC – Load Regulation Performance 2.5-V VOUT, PFM Mode – TPS62230
Figure 49. Load Transient Response 5 mA to 150 mA, PFM to PWM Mode, VOUT 1.8 V – TPS62231
Figure 51. Load Transient Response 5 mA to 200 mA, PFM to PWM Mode, VOUT 2.5 V – TPS62230
Figure 50. Load Transient Response 5 mA to 150 mA, Forced PWM Mode, VOUT 1.8 V – TPS62231
Figure 52. Load Transient Response 5 mA to 200 mA, Forced PWM Mode, VOUT 2.5 V – TPS62230
Figure 53. TPS62231 1.8-V Output
Figure 54. TPS62232 1.2-V Output