SLVK198A July   2025  – August 2025 TPS7H3014-SEP

 

  1.   1
  2.   2
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Depth, Range, and LETEFF Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-Up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
  12. 9 Event Rate Calculations
  13. 10Summary
  14.   A References
  15.   B Revision History

Test Setup and Procedures

There were four input supplies used to provide power to the TPS7H3014-SEP. The voltage values and the model of the used equipment per the SEE test type is presented in Table 6-1.

Table 6-1 Details of Power Supplies Used for the Heavy-Ion Test Campaign of the TPS7H3014-SEP
VOLTAGE NAMEVOLTAGE (V)SEE TEST TYPEPOWER SUPPLY MODEL

VIN

14

SEL, SEB/SEGR

N6766A

VPULL_UP1

7

PXIe-4139

VPULL_UP2

7

VUP

0, 3.3

VIN

5

SET

N6766A

VPULL_UP1

3.3

PXIe-4139

VPULL_UP2

3.3

VUP

0, 1

As discussed in Section 3 the TPS7H3014-SEP was tested (or evaluated) under heavy-ions using three unique configurations.

  1. For DSEE the device was tested under the configuration shown in Figure 3-3. We refer to this configuration as the loopback. In loopback mode ENx is connected to SENSEx via a resistor divider for automatic sequence up and down. ENX was tied to SENSEX using a resistor divider with RTOP = 100kΩ and RBOTTOM = 21kΩ. Under this configuration the overdrive The overdrive is referring to the difference between the steady-state voltage when the hysteresis current is active and the internal VTH_SENSEx reference voltage (599mV typically). For example, for an overdrive voltage of 1V the steady-state voltage is 1.599V when the IHYS_SENSEx is active. voltage is 1V (typically).
  2. For SET the device was tested under the configuration shown in Figure 3-4. This testing was completed in the loopback configuration. ENX was tied to SENSEX using a resistor divider with RTOP = 1.91kΩ and RBOTTOM = 976Ω. Under this configuration the overdrive voltage is ±20mV (typically). The device was tested under:

    1. Waiting to Sequence UP State (with –20mV).
    2. Waiting to Sequence DOWN State (with+20mV).

Transients were monitored on EN1, EN4, and FAULT. The equipment used and the trigger details are summarized in Table 6-2. The device was tested for transients under the Waiting to Sequence UP and Waiting to Sequence DOWN states. This was done to ensure the device will not activate/deactivate any downstream device (typically a POL) connected to it.

Table 6-2 Summary of Oscilloscope and Conditions Used for the SEE Test Campaign of the TPS7H3014-SEP

SIGNAL NAME

EQUIPMENT USED TO MONITOR SIGNAL

TRIGGER TYPE

TRIGGER VALUE

WHEN SIGNAL WAS HIGH (%)

TRIGGER VALUE

WHEN SIGNAL WAS LOW (V)

EN1

PXIe-5172

Falling, edge

Rising, edge

–20 (from nominal)

0.66, 0.36

EN4

PXIe-5172

Falling, edge

Rising, edge

–20 (from nominal)

0.66, 0.36

FAULT

PXIe-5172

Falling, edge

–20 (from nominal)

0.66, 0.36

Figure 6-1 shows a block diagram of the setup used for SEE testing of the TPS7H3014-SEP.

All boards used for SEE testing were fully checked for functionality. Dry runs were also performed to ensure that the test system was stable under all bias and load conditions prior to being taken to the test facilities. During the heavy-ion testing, the LabVIEW control program powered up the TPS7H3014-SEP device and set the external sourcing and monitoring functions of the external equipment. After functionality and stability was confirmed, the beam shutter was opened to expose the device to the heavy-ion beam. The shutter remained open until the target fluence was achieved (determined by external detectors and counters). During irradiation, the NI scope cards continuously monitored the signals. When the output exceeded the pre-defined 20% edge trigger, a data capture was initiated. No sudden increases in current were observed (outside of normal fluctuations) on any of the test runs and indicated that no SEL or SEB/SEGR events occurred during any of the tests. Neither, a single transient was capture by the oscilloscope measuring the outputs indicting the device is SET-free.

TPS7H3014-SEP Block Diagram of the SEE Test Setup for the TPS7H3014-SEPFigure 6-1 Block Diagram of the SEE Test Setup for the TPS7H3014-SEP