• Menu
  • Product
  • Email
  • PDF
  • Order now
  • How TPSI3133 DESAT Can Protect Your Expensive SiC MOSFETs and IGBTs

    • SLVAG18 April   2025 TPSI3100 , TPSI3100-Q1

       

  • CONTENTS
  • SEARCH
  • How TPSI3133 DESAT Can Protect Your Expensive SiC MOSFETs and IGBTs
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Why DESAT Protection Is Needed
    1. 1.1 Key Considerations for DESAT Protection
  5. 2Key DESAT Circuit Components
    1. 2.1 Circuit Startup Behavior
  6. 3Design Example
    1. 3.1 Design Requirements
    2. 3.2 Threshold Equations
    3. 3.3 Given Parameters
    4. 3.4 Inserting Given Parameters into Equations
    5. 3.5 Solving Equations for Unknowns
    6. 3.6 Selecting Resistances to Satisfy Equations
    7. 3.7 Determining Blanking Capacitance
    8. 3.8 Final Component Values
    9. 3.9 Lab Testing
  7. 4Closing
  8. IMPORTANT NOTICE
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
Application Note

How TPSI3133 DESAT Can Protect Your Expensive SiC MOSFETs and IGBTs

Abstract

Protecting power semiconductors like SiC MOSFETs and IGBTs from damage due to oversaturation is critical in power electronics design. When these devices perform beyond their intended operating region, excessive power dissipation can lead to thermal stress and failure.

Desaturation (DESAT) protection circuits offer cost-effective protection by monitoring the voltage across the semiconductor and shutting it down during an overcurrent event. This article explores how DESAT protection works, key circuit components, and how to design a DESAT circuit with the TPSI3133 isolated switch driver.

Trademarks

All trademarks are the property of their respective owners.

1 Why DESAT Protection Is Needed

Power semiconductors like MOSFETs and IGBTs ideally operate in a fully saturated state: ohmic region for MOSFETs and saturation region for IGBTs. The voltage across, VDS for MOSFETs or VCE for IGBTs, remains low to minimize power dissipation. However, when these devices enter an oversaturated state as shown in Figure 1-1, small increases in current cause large voltage increases, leading to excessive power dissipation and potential damage.

 Example IGBT I-V Curve Figure 1-1 Example IGBT I-V Curve

Some isolated switch drivers include a desaturation (DESAT) protection feature that monitors VDS or VCE and quickly shuts down the semiconductor during an overcurrent event. The TPSI31xx is a family of fully integrated isolated switch drivers, which when combined with an external power switch, forms a complete isolated solid-state relay solution.

The TPSI3133, as shown in Figure 1-2, is a variant specifically intended for DESAT due to its internal pulldown MOSFET on the fault comparator input. This internal MOSFET prevents false positives while the IGBT/SiC MOSFET is off by pulling down the fault comparator input and keeping it pulled down for an additional 100ns after EN goes high, allowing the IGBT/SiC MOSFET to fully turn on.

 DESAT With TPSI3133 Figure 1-2 DESAT With TPSI3133

1.1 Key Considerations for DESAT Protection

DESAT protection circuits are typically configured with IGBTs because IGBTs show distinct voltages (VCE) across current (IC) in the saturation region which makes detection easier, have sharper transitions into the active region, and generally able to handle more power due to larger die size (many have a short circuit withstand rating).

DESAT can also work with SiC MOSFETs. The problem with low voltage MOSFETs is since the overcurrent threshold is typically set well above normal operation to avoid false positives, a low voltage MOSFET may be damaged by overheating well before the circuit even detects an overcurrent event.

By implementing DESAT protection, engineers can ensure power semiconductors stay within safe operating area.

2 Key DESAT Circuit Components

  1. Blocking diode: Protects the circuit from high voltage while the IGBT/SiC MOSFET is off.
  2. Current limiting resistor (RLIM) to limit diode forward current.
  3. DESAT threshold detection (RDIV1, RDIV2): Defines the voltage threshold for detecting oversaturation.
  4. Blanking capacitance (CBLK): Filters noise and prevents false triggering. While blanking capacitance helps avoid false positives, it may also extend stress time on the IGBT/SiC MOSFET during overcurrent events.

2.1 Circuit Startup Behavior

At power-up while EN is low, TPSI3133 receives power and begins to transfer power to its secondary rails (VDDM and VDDH). The internal MOSFET pulls down the comparator input to avoid a false trigger. Once EN goes high, the two current paths (paths 1 and 2) compete to set the comparator input voltage as shown in Figure 2-1. Since Path 1 normally would be faster than path 2 due to IGBT turn-on delay, once EN goes high, the TPSI3133 keeps the comparator input pulled down for an additional 100ns, allowing the IGBT to fully turn on before fault detection. Adding blanking capacitance (CBLK) can provide additional delay but must be carefully selected in order to minimize stress time. During an overload condition, the IGBT VCE rises, which brings up the voltage at the HV diode anode, trips the fault comparator threshold. Once the TPSI3133 detects the fault, it shuts off the driver which turns off the IGBT, protecting the system.

 DESAT KVL Paths Figure 2-1 DESAT KVL Paths
Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale