SLVAFD6 July   2022 TPS564247 , TPS565242

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Analysis of the Floating-Input Pre-bias Output Operation
    1. 2.1 Analysis of FCCM Device
    2. 2.2 Analysis of PSM Device
  5. 3Experimental Verification
    1. 3.1 FCCM device
      1. 3.1.1 Bias Voltage > Target
      2. 3.1.2 Bias Voltage < Target
    2. 3.2 PSM device
      1. 3.2.1 Bias Voltage > Target
      2. 3.2.2 Bias Voltage < Target
  6. 4Summary
  7. 5References

Analysis of FCCM Device

As mentioned above, FCCM device doesn’t have the ZC logic. It means that the turn on time of high side MOSFET and the low side MOSFET is complemented, if deadtime is neglected. Figure 2-1 shows the basic logic block of adaptive constant on-time (D-CAP™) control [3], when analysis the FCCM device, the ZC part can be neglected.

Figure 2-1 D-CAP™ Mode With Adaptive On-Time Modulator Block Diagram

From the operation logic of D-CAP structure, the device will compare the output feedback (FB) and reference voltage (Ref), the high side MOSFET will turn on when bias output voltage is lower than the target. If the bias output voltage is higher than target, high side will turn off and the lower side will turn on. The inductor current will ramp down, until it triggers negative operation current (NOC) protection. Because the logic priority of NOC is higher than the above compare logic, after triggering NOC, high side MOSFET will turn on, and the on time is same as the normal operation which is relative to input voltage Vin and output voltage Vout, as shown in the Equation 2.

Equation 2. T on = V bias V in * F sw

Where Fsw=1/(Ron*Con), shown in Figure 2-1.

Because high side will turn on and transfer negative current to Vin side. It is difficult to judge the final state of Vin by a direct logic, so the hypothetical backstepping logic can be used. Suppose Vin can be a stable and constant voltage finally. Because there is no load in Vin side, so if Vin can be stable, the average inductor current must be zero. It means the absolute value of peak inductor current and valley inductor current is same, as shown in Figure 2-2.

Figure 2-2 Supposed Stable Waveform of FCCM Mode, Vout > Target

From Figure 2-2, the turn-off time of high side switch is show in following.

Equation 3. T off = 2LI NOC V bias

From the basic relationship between Vin and Vout, Vin is shown in following formula.

Equation 4. V in = V bias 1- t off t off + t on

Substitute Equation 2, Equation 3 into Equation 4, Vin can be written as Equation 5.

Equation 5. V in = T s V bias 2 V bias / F sw - 2LI NOC

From Equation 5, the stable value of Vin is related to INOC and inductor value L. If Vbias/Fsw<=2LINOC, it means Vin can be stable with a non-infinite constant value; if Vbias/Fsw>2LINOC, Vin can be a stable with a constant value, but it is determined by INOC and L. Generally, Vbias/Fsw-2LINOC is a small value if the converter is reasonably designed, so Vin may be very large in this condition. So there exists the risk of over voltage damage.

If the output voltage is lower than the target, the minimum off time of high-side switch will always be triggered. So, on time is same as Equation 3, off time is shown in Equation 6. In steady sate, the voltage-second balance is established, as shown in Equation 7. By substitute Equation 2, Equation 6 into Equation 7, Vin can be written as Equation 8. Generally, the minimum off time is much smaller than 1/Fsw, so Vin will be closed to Vbias. It is not a high value that can casue damage.

Equation 6. Toff=Toff_min
Equation 7. Vin-Vbias*Ton/L=Vbias*Toff/L
Equation 8. V in = V bias (1- F sw *T off_min )

Although the input voltage will not be a high value if Vout <Vtarget. But if consider the regulation and fluctuation, the operation of FCCM device has relative high risk of damage on the whole. Because the input voltage may ramp up to a very high value. For FCCM device, it suggests to use Enable function to shut down itself, and keep the bias standby operation safety. Most of TI's power DC/DC device support the enable function, can control the operate and shut down of converter flexibility.