SLVAER2A April   2020  – November 2020 TPS50601-SP , TPS50601A-SP

 

  1.   Trademarks
  2. 1Introduction
  3. 2Overview
  4. 3Schematic and Layout Changes
  5. 4References
  6. 5Revision History

Schematic and Layout Changes

Most designs will need very little change to upgrade from the TPS50601-SP. The package pictures of the devices are shown in Figure 3-1 and Figure 3-2. While the devices are mechanically the same, pin 16 is different between the two devices. The TPS50601-SP has pin 16 as a bootstrap pin for the high-side nFET, and the TPS50601A-SP has a pin to place a capacitor to help stabilize the reference voltage. For layout, the TPS50601-SP requires a 0.1-μF ceramic capacitor to be placed between the pin and the PH node, while the TPS50601A-SP requires a 470-μF ceramic capacitor from the pin to ground. If all the component value changes have a comparable footprint, this is the only layout change needed between the two devices.

GUID-887A1349-8FB4-44B9-AE9E-BBE00EE45B29-low.pngFigure 3-1 TPS50601-SP Pin Out Diagram
GUID-D0A1AC61-4EEF-4A09-9784-8222C2846D93-low.pngFigure 3-2 TPS50601A-SP Pin Out Diagram