SLUUCP2 June   2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Required Data
  4. 2Data Submission
  5. 3Revision History

Data Submission

The zip file created as previously described must be submitted to the GPC tool through the web interface here: https://www.ti.com/powercalculator/docs/gpc/gpcUpload.tsp. After processing, an e-mail with a report that includes the calculated coefficients is sent to the e-mail address you provide when logging in. The report contains the log file, calculated coefficients, and graph showing the expected performance of the calculated coefficients. If any format or other errors are present, they are reflected in the report.

If using the 18-k pullup option, enter these numbers into the Calibration:18K Temperature Model register settings for the BQ769x2 device. If using the 180-k pullup option, enter these numbers into the Calibration:180K Temperature Model register settings. When configuring the thermistor pins, make sure to select the correct temperature model using the OPT[3:2] bits for the pin configuration registers.