SLUUCK4 November   2021

 

  1. 1Introduction
  2. 2Performance Specification Summary
  3. 3Modifications
    1. 3.1 MODE Pin Configuration
    2. 3.2 Output Voltage Setpoint
  4. 4Test Setup
    1. 4.1 Input/Output Connections
    2. 4.2 Start-Up Procedure
  5. 5Board Layout
    1. 5.1 Layout
    2. 5.2 EVM Picture
  6. 6Schematic, List of Materials, and Reference
    1. 6.1 Schematic
    2. 6.2 List of Materials
  7. 7Reference

Layout

The board layout for the TPS562212EVM is shown in Figure 5-1, Figure 5-2, and Figure 5-3. The top layer contains the main power traces for VIN, VOUT, and ground. Also on the top layer are connections for the pins of the TPS562212 and a large area filled with ground. Most of the signal traces are also located on the top side. The input decoupling capacitors, C1, C2, and C3, are located as close to the IC as possible. The input and output connectors, test points, and all of the components are located on the top side. The bottom layer is a ground plane along with the switching node copper fill, signal ground copper fill and the feedback trace from the point of regulation to the top of the resistor divider network. Both the top layer and bottom layer use 2-oz copper thickness.

GUID-20211117-SS0I-8QRD-5DB1-XF4HJWHSRXB7-low.jpgFigure 5-1 TPS562212EVM Top Assembly
GUID-5AEE0592-DF43-4769-9317-D3AB242404EC-low.gifFigure 5-2 TPS562212EVM Top Layer
GUID-D3091D30-4E2E-4D4E-B6BE-3948B207CB56-low.gifFigure 5-3 TPS562212EVM Bottom Layer