SLUUC88B March   2021  – November 2021 TPS62869

 

  1. 1Introduction
    1. 1.1 Performance Specification
    2. 1.2 Modifications
  2. 2Setup
    1. 2.1 Input/Output Connector Descriptions
    2. 2.2 Hardware Setup
  3. 3TPS62869EVM-118 Test Results
  4. 4Board Layout
  5. 5Schematic and List of Materials
    1. 5.1 Schematic
    2. 5.2 List of Materials
  6. 6Software User Interface
    1. 6.1 Software Setup
    2. 6.2 Interface Hardware Setup
    3. 6.3 User Interface Operation
      1. 6.3.1 Home Screen
      2. 6.3.2 Settings Screen
  7. 7Revision History

User Interface Operation

Upon start-up, the GUI automatically connects to the EVM. If not, click on the Connect button in the upper right corner of the GUI window. Ensure the I²C Slave Address is correct. The following sections give a short overview of the two main GUI screens.