SLUS987C January 2011 – December 2019
PRODUCTION DATA.
The BQ33100 is a super capacitor monitor, balancing controller, and overall system manager. The device can individually monitor up to five series capacitors and up to nine when monitoring the total stack.
The device can also interact with an external charging solution to provide capacitance and effective series resistance (ESR) data on the stack.
NOTE
The following notation is used in this document if SBS commands and data flash values are mentioned within a text block:
All SBS commands, data flash values and flags mentioned in a chapter are listed at the beginning of each chapter for reference.
The reference format for SBS commands is:
SBS:Command Name(Command No.):Manufacturer Access(MA No.)[Flag], for example:
SBS:Voltage(0x09), or SBS:ManufacterAccess(0x00):Seal Device(0x0020)