SLUAAL4 August   2022 BQ21040

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2How Temperature Sensing Works on the BQ21040
    1. 2.1 With Adapter Present
    2. 2.2 Without Adapter Present
  5. 3Example Application
    1. 3.1 Required Devices
    2. 3.2 Setup
  6. 4Procedure
    1. 4.1 Detecting Adapter Removal
    2. 4.2 Detecting Adapter Insertion
    3. 4.3 Logical Flowchart
  7. 5Summary
  8. 6References

Logical Flowchart

Figure 4-1 outlines the basic logical procedure that needs to be implemented on the MCU to properly detect adapter insertion and removal.

Figure 4-1 Logical Flowchart