SLUAAA8 November   2020 UCC28740-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the UCC28740-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the UCC28740-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the UCC28740-Q1 data sheet.

GUID-1CE147D2-FA63-4B65-A74D-951D5345348E-low.gif Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device is connected according to the design procedure application example shown in Figure 19, in UCC28740-Q1 datasheet
  • The supply pin refers to VDD pin
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VDD1Device is not functional, system will not startup.B
VS2IC remains in input under voltage protection mode. The output of the flyback converter remains at zero.B
FB3 Device operates at its maximum switching frequency with maximum duty cycle. Output OVP is triggered.B
GND 4 No effect. D
CS 5 When CS pin is shorted to ground before the IC startup, CS pin short protection. The output of the flyback converter remains at zero. B
When CS pin is shorted to ground after the IC in operation, potnetial power stage damange and it might cause IC damage. A
DRV 6 DRV remains low. The output of the flyback converter remains at zero. B
N/A 7
HV 8 The VDD capacitor cannot be trickle charged and the converter will never startup. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VDD1No positive supply applied to device, device is not functional.B
VS 2 IC remains in input under voltage protection mode. The output of the flyback converter remains at zero. B
FB 3 Device operates at its maximum switching frequency with maximum duty cycle. Output OVP is triggered. B
GND 4 Device Damage A
CS 5 CS pin open protection. The output of the Flyback converter remains at zero. B
DRV 6 The output of the Flyback converter remains at zero. B
N/A7
HV8The VDD capacitor cannot be trickle charged. Output of the converter remains at zero volts.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VDD1VSVS max voltage rating exceeded, device damaged, possible Flyback switch damageA
VS 2 FB FB will not be stable, output voltage will not regulate correctly C
FB 3 GND Device operates at maximum switching frequency with maximum duty cycle. Output over voltage protection will be triggered B
GND 4 N/A
CS 5 DRV CS max voltage rating will be exceeded, device damage, possible Flyback switch damage A
DRV 6 N/A
N/A7N/A
HV8N/A
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VDD1No Effect.D
VS 2 Pin's maximum voltage rating exceeded, posibble IC damage. A
FB 3 Pin's maximum voltage rating exceeded, posibble IC damage. A
GND 4 No positive supply applied to device. Device is non-functional. B
CS 5 DRV remains low. Possible IC damage. A
DRV 6 DRV remains high. Possible IC damage and Flyback switch damage. A
N/A7
HV8The max rating of VDD will be exceeded, possible device damage and Flyback switch damage.A