SLUA790 November 2016 BQ34110 , BQ34Z100-G1 , BQ35100
Read these like Standard Commands. As an example, use the State-of-Health (SOH), its command code is 2E/2F.
Use the I2C Master Control Panel section to read the flash.
ENTER: Start Register 2E, Number of Bytes to Read 2, and PRESS the Read button.
Figure 5. Extended I2C Command Reading State-of-Health Byte swap the data and convert it to decimal. 0062 is 98% SOH.