SLOS739A July 2012 – March 2016
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The typical connection diagram highlights the required external components and system level connections for proper operation of the device in several popular system examples.
Each of these configurations can be realized using the Evaluation Module (EVM) for the device. These flexible modules allow full evaluation of the device in the most common modes of operation. Any design variation can be supported by TI through schematic and layout reviews. Visit http://e2e.ti.com for design assistance and join the audio amplifier discussion forum for additional information.
Figure 71. Mono PBTL System With Headphone Driver
Table 25 lists the design parameters of the TAS5721.
| PARAMETER | EXAMPLE |
|---|---|
| Low Power Supply | 3.3 V |
| High Power Supply | 8 V to 24 V |
| Host Processor | I2S Compliant Master |
| I2C Compliant Master | |
| GPIO Control | |
| Output Filters | Inductor-Capacitor Low Pass Filter(1) |
| Speaker | 8 Ω minimum BTL 4 Ω minimum PBTL and Single Ended |
The typical connections required for proper operation of the device can be found on the TAS5721EVM User’s Guide (SLOU346). The device was tested this this list of components, deviation from this typical application components unless recommended by this document may produce unwanted results, which could range from degradation of audio performance to destructive failure of the device. The application report SLOA119 offers a detailed description on proper component selection and design of the output filter based upon the modulation used, desired load and response.
Customary pullup resistors are required on the SCL and SDA signal lines. They are not shown in the Typical Application Circuits, because they are shared by all of the devices on the I²C bus and are considered to be part of the associated passive components for the System Processor. These resistor values should be chosen per the guidance provided in the I²C Specification.
The digital I/O lines of the TAS5721 are described in previous sections. As discussed, whenever a static digital pin (that is a pin that is hardwired to be HIGH or LOW) is required to be pulled HIGH, it should be connected to DVDD through a pullup resistor to control the slew rate of the voltage presented to the digital I/O pins. It is not, however, necessary to have a separate pullup resistor for each static digital I/O line. Instead, a single resistor can be used to tie all static I/O lines HIGH to reduce BOM count.
Figure 72. Recommended Command Sequence
Figure 73. Power Loss Sequence
Use the following sequence to power-up and initialize the device:
The following are the only events supported during normal operation:
NOTE
Event 3 is not supported for 240 ms + 1.3 × tstart after trim following AVDD/DVDD powerup ramp (where tstart is 300 ms when mid-Z ramp is enabled and is otherwise specified by register 0x1A).
Enter:
Exit:
Use the following sequence to powerdown the device and its supplies:
Figure 74. Output Power vs PVDD in 2.1 Mode
Figure 76. Crosstalk vs Frequency in 2.0 Mode
Figure 75. Efficiency vs Output Power in 2.0 Mode
Figure 77. Typical Application Circuit for Stereo (BTL) Configuration
Figure 78. 2.1 System With Headphone Driver
Figure 79. Stereo (BTL) System
Figure 80. Mono (PBTL) System
Figure 81. 2.1 System