SLLU248B July   2016  – August 2016

 

  1.   USB Type-C Mini Dock EVM
    1.     Trademarks
    2. 1 What is the TI USB Type-C Dock?
    3. 2 TI USB Type-C Mini Dock Features
    4. 3 USB Type-C Mini Dock Quick-Start Guide
    5. 4 Schematics
  2.   Revision History

USB Type-C Mini Dock Quick-Start Guide

The following steps are provided for a quick-start using the EVM:

  1. Connect the USB Type-C Enabler Board to the PC with a USB Type-A to USB-B cable and a DisplayPort Cable.
  2. Connect the USB Type-C Enabler Board to the USB Type-C Mini Dock EVM with a USB Type-C cable.
  3. fig03_sllu248.jpgFigure 3. USB Type-C Dock Example Setup
  4. Confirm that D822, D826, D824, D827, D820, D829 are lit.
  5. fig04_sllu248.jpgFigure 4. USB Type-C Dock Example Setup
    fig05_sllu248.jpgFigure 5. USB Type-C Dock Example Setup
  6. Connect the Dell power adapter and confirm that the D823, D825, D824, D827, D820, D829 are lit.
  7. Connect a USB flash drive to the USB Type-C Mini Dock EVM and confirm that data can be transferred to and from the USB flash drive.
  8. Connect the HDMI cable to the USB Type-C Mini Dock EVM and to a monitor, confirm PC video is displayed on the monitor.
  9. Disconnect the HDMI cable and connect a miniDP cable to the USB Type-C Mini Dock EVM and to a monitor, confirm PC video is displayed on the monitor.