SLDU019B December 2015 – March 2016
The PGA450Q1EVM-S is preloaded with the EEPROM values listed in Table 2. These instructions are provided in the event that the user prefers to modify the EEPROM using the PGA450Q1EVM GUI, rather than the corresponding UART command. Use the steps that follow to program the device for EEPROM memory.
The values at 0x00 to 0x1F are the threshold values used in software. TI recommends that the user begins with the example values provided, and then adjusts these values later as necessary.
The value at address 0x1F is the sensor address.
| Register Address | Register Value | Description |
|---|---|---|
| 0x00 | 0xFF | Threshold level 0 |
| 0x01 | 0xD7 | Threshold level 1 |
| 0x02 | 0x95 | Threshold level 2 |
| 0x03 | 0x84 | Threshold level 3 |
| 0x04 | 0x62 | Threshold level 4 |
| 0x05 | 0x62 | Threshold level 5 |
| 0x06 | 0x52 | Threshold level 6 |
| 0x07 | 0x78 | Where in FIFO to apply threshold level 7 defined at EEPROM address 0x08 from to the end of the FIFO. Long mode (most significant hex) multiplied by 40 [interval 40 to 600]. Short mode (least significant hex) multiplied by 8 [interval 8 to 120]. |
| 0x08 | 0x64 | Threshold level 7, the fixed level of threshold to end of FIFO. Long mode and short mode multiplied by 5 and 1 respectively. |
| 0x09 | 0x95 | Threshold ignore count from beginning of FIFO for long (most significant hex) and short (least significant hex) modes respectively. |
| 0x0A | 0x43 | 1-6 change interval of the threshold level across FIFO for long mode (most significant hex) multiplied by 8 [interval 8 to 120]. Short mode (least significant hex) multiplied by 2 [interval 2 to 15]. |
| 0x0B | 0x12 | PULSE_CNTA |
| 0x0C | 0xFF | BLANKING_TIMER |
| 0x0D | 0x06 | FIFO_CTRL |
| 0x0E | 0x32 | DOWNSAMPLE |
| 0x0F | 0x01 | CONTROL_1 |
| 0x10 | 0x00 | BURST_MODE |
| 0x11 | 0x8A | BURST_ONA_LSB |
| 0x12 | 0x8A | BURST_OFFA_LSB |
| 0x13 | 0x05 | DEADTIME |
| 0x14 | 0x09 | SAT_DEGLITCH |
| 0x15 | 0x03 | BPF_B1_MSB |
| 0x16 | 0x2D | BPF_B1_LSB |
| 0x17 | 0xEC | BPF_A2_MSB |
| 0x18 | 0x3D | BPF_A2_LSB |
| 0x19 | 0xF9 | BPF_A3_MSB |
| 0x1A | 0xA5 | BPF_A3_LSB |
| 0x1B | 0x35 | LPF_B1_MSB |
| 0x1C | 0xDD | LPF_B1_LSB |
| 0x1D | 0x14 | LPF_A2_MSB |
| 0x1E | 0x46 | LPF_A2_LSB |
| 0x1F | 0x01 | Sensor address |