SLAZ771 February   2026 MSPM0G1218 , MSPM0G3218-Q1

 

  1.   1
  2.   Abstract
  3. 1Functional Advisories
  4. 2Preprogrammed Software Advisories
  5. 3Debug Only Advisories
  6. 4Fixed by Compiler Advisories
  7. 5Device Nomenclature
  8. 6Advisory Descriptions
    1. 6.1  AES_ERR_01
    2. 6.2  CPU_ERR_02
    3. 6.3  CPU_ERR_03
    4. 6.4  FLASH_ERR_03
    5. 6.5  FLASH_ERR_04
    6. 6.6  FLASH_ERR_05
    7. 6.7  FLASH_ERR_08
    8. 6.8  GPIO_ERR_05
    9. 6.9  GPIO_ERR_06
    10. 6.10 KEYSTORE_ERR_01
    11. 6.11 MATHACL_ERR_01
    12. 6.12 PMCU_ERR_13
    13. 6.13 RST_ERR_01
    14. 6.14 SYSCTL_ERR_01
    15. 6.15 SYSCTL_ERR_02
    16. 6.16 SYSCTL_ERR_03
    17. 6.17 SYSCTL_ERR_04
    18. 6.18 SYSCTL_ERR_05
    19. 6.19 SYSCTL_ERR_06
    20. 6.20 SYSOSC_ERR_01
    21. 6.21 SYSOSC_ERR_02
    22. 6.22 SYSOSC_ERR_04
    23. 6.23 SYSPLL_ERR_01
    24. 6.24 TIMER_ERR_04
    25. 6.25 TIMER_ERR_06
    26. 6.26 TIMER_ERR_07
    27. 6.27 UNICOMMI2CC_ERR_01
    28. 6.28 UNICOMMUART_ERR_06
    29. 6.29 UNICOMMUART_ERR_07
    30. 6.30 UNICOMMUART_ERR_09
    31. 6.31 UNICOMMUART_ERR_10
    32. 6.32 VREF_ERR_05
  9. 7Revision History

FLASH_ERR_04

FLASH Module

Category

Functional

Function

Wrong Address gets reported in the SYSCTL->DEDERRADDR

Description

When a FLASHDED error appears the data truncates the most significant byte. In the memory limits of the device, the most significant byte does not have an impact to the return address for MAIN flash. For NONMAIN flash or Factory region the MSB can be listed as 0x41xx.xxxx

Workaround

If the return address of the SYSCTL_DEDERRADDR returns a 0x00Cxxxxx, do an OR operation with 0x41000000 to get the proper address for the NONMAIN or Factory region return address. For example, if SYSCTL_DEDERRADDR = 0x00C4013C, the real address is 0x41C4013C.

For MAIN Flash DED, the SYSCTL_DEDERRADDR can be used as is.