SLAZ771 February   2026 MSPM0G1218 , MSPM0G3218-Q1

 

  1.   1
  2.   Abstract
  3. 1Functional Advisories
  4. 2Preprogrammed Software Advisories
  5. 3Debug Only Advisories
  6. 4Fixed by Compiler Advisories
  7. 5Device Nomenclature
  8. 6Advisory Descriptions
    1. 6.1  AES_ERR_01
    2. 6.2  CPU_ERR_02
    3. 6.3  CPU_ERR_03
    4. 6.4  FLASH_ERR_03
    5. 6.5  FLASH_ERR_04
    6. 6.6  FLASH_ERR_05
    7. 6.7  FLASH_ERR_08
    8. 6.8  GPIO_ERR_05
    9. 6.9  GPIO_ERR_06
    10. 6.10 KEYSTORE_ERR_01
    11. 6.11 MATHACL_ERR_01
    12. 6.12 PMCU_ERR_13
    13. 6.13 RST_ERR_01
    14. 6.14 SYSCTL_ERR_01
    15. 6.15 SYSCTL_ERR_02
    16. 6.16 SYSCTL_ERR_03
    17. 6.17 SYSCTL_ERR_04
    18. 6.18 SYSCTL_ERR_05
    19. 6.19 SYSCTL_ERR_06
    20. 6.20 SYSOSC_ERR_01
    21. 6.21 SYSOSC_ERR_02
    22. 6.22 SYSOSC_ERR_04
    23. 6.23 SYSPLL_ERR_01
    24. 6.24 TIMER_ERR_04
    25. 6.25 TIMER_ERR_06
    26. 6.26 TIMER_ERR_07
    27. 6.27 UNICOMMI2CC_ERR_01
    28. 6.28 UNICOMMUART_ERR_06
    29. 6.29 UNICOMMUART_ERR_07
    30. 6.30 UNICOMMUART_ERR_09
    31. 6.31 UNICOMMUART_ERR_10
    32. 6.32 VREF_ERR_05
  9. 7Revision History

FLASH_ERR_05

FLASH Module

Category

Functional

Function

DEDERRADDR can have incorrect reset value

Description

The reset value of the SYSCTL->DEDERRADDR can return a 0x00C4013C instead of the correct 0x00000000. The location of the error is in the Factory Trim region and is not indicative of a failure, it can be properly ignored. The reset value tends to change once NONMAIN has been programmed on the device.

Workaround

Accept 0x00C4013C as another reset value, so the default value from boot can be 0x00000000 or 0x00C4013C. The return value is outside of the range of the MAIN flash on the device so there is no potential of this return coming from an actual FLASH DED status.