SLAZ734B February 2020 – August 2021 MSP430FR6005
USCI Module
Functional
Interrupt Flag polling can cause unrpedictable behavior if eUSCI is running with different clock then CPU
If the interrupt flags e.g. UCAIFG of the eUSCI are polled via the CPU during a while loop or during the following assembly instruction the CPU behavior can become unpredictable when the corresponding interrupt flag is set asynchronously during the execution of the bit instruction. The corresponding CPU flags used by the conditional jump can become unstable causing unpredictable CPU execution.
CHECK_FLAG
BIT.W #8,&UCAxIFG
JEQ CHECK_FLAG
Buffer the interrupt flag which should be polled, to a CPU internal register e.g. R15 and use this register for the decision (bit + jeq).
The bit of interest remains stable during the CPU decision because the value is settled in the CPU internal register.
In C, declaring the buffer variable as volatile avoids compiler optimizations that may result in the assembly code above.
Workaround in C:
volatile unsigned short flag;
do
{
flag = UCA0IG;
}while ((flag & UCRXIFG) == 0x00);
Workaround in asm:
PUSH R15
loop:
MOV.W &UCAxIFG, R15
BIT.W #8,R15
JEQ loop
POP R15