SFFSB65 March   2026 BQ24078

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Pin Failure Mode Analysis (Pin FMA)
  6. 4Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the BQ24078. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 3-2 through Table 3-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 3-1.

Table 3-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 3-1 shows the BQ24078 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the BQ24078 datasheet.

BQ24078 Pin DiagramFigure 3-1 Pin Diagram
Table 3-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
TS1The charger in the hot region of the TS pin stops charging.B
BAT2The device stops charging when the battery voltage is below the VBAT(SC) short-circuit protection. There is uncontrolled current from the battery to the ground.B
3
CE4The charger is active.D
EN25The input current limit is set to either USB100 or USB500 mode. Refer to the EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet.C
EN16The input current limit is set to either USB100 or ILIM mode. Refer to the EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet.C
PGOOD7The PGOOD LED is always on. An incorrect PGOOD status is reported. The charge function of the device is still functional.C
VSS8The VSS pin is GND.D
CHG9The CHG LED is always on. An incorrect charger status is reported. The charge function of the device is still functional.C
OUT10OUT short-circuit recovery is active when VOUT < VO(SC1). The input current is limited to 100mA.B
11
ILIM12The input current is not limited when the ILIM pin is shorted to ground after start-up. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device. When the short is removed, the device operates as normal. When a short occurs before start-up, the device does not charge.A
IN13The input FET is turned off. The output is powered by the battery. There is uncontrolled current from the input supply.B
TMR14The safety timer is disabled. The charge function of the device is still functional.C
SYSOFF15The BATFET (battery field-effect transistor) operates normally.D
ISET16The charging function is disabled. The device resumes charging when the short is removed.D
Table 3-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
TS1The charging function is disabled. The voltage of the TS pin pulls high due to the 75µA current source, which puts the voltage of the TS pin outside the charge range.B
BAT2The device stops charging. The charger goes into battery-detect mode. The OUT pin is powered by the IN pin.D
3
CE4There is 285kΩ of internal pulldown on the CE pin. The device is enabled and charging occurs.D
EN25There is 285kΩ of internal pulldown on the EN2 pin. The input current limit is dependent on the EN1 and EN2 pins, according to the EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet.C
EN16There is 285kΩ of internal pulldown on the EN1 pin. The input current limit is dependent on the EN1 and EN2 pins, according to the EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet.C
PGOOD7There is an open-drain output. There is no PGOOD indication. The charger functions normally.D
VSS8The device is off and inactive.B
CHG9This pin is an open-drain output. There is no charge status indication. The charger functions normally.D
OUT10There is no load on the OUT pin. The charger functions normally.D
11
ILIM12The input FET is turned off. The OUT pin is powered by the BAT pin.B
IN13There is no input. The OUT pin is powered by the battery.D
TMR14The safety timer is set to default values. The device stops charging after the timer expires.D
SYSOFF15The BATFET is off. The SYSOFF pin is internally pulled up to VBAT through a large resistor (approximately 5MΩ), and the BATFET turns off when the SYSOFF pin is high.C
ISET16The charging current is set to 0mA. The OUT pin is powered by the input or battery.B
Table 3-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
TS1BATThe device stops charging. The voltage of the TS pin is outside the charging range.B
BAT3CEThe CE pin is pulled high, and charging is disabled.B
EN25EN1The input current limit is set to either USB100 mode (if both pins are pulled low) or USB suspend mode (if both pins are pulled high as stated in the EN1/EN2 Settings table in the Pin Configuration and Functions section of the data sheet).C
EN16PGOODThe EN1 pin is pulled low when VIN is present. The EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet states the state of the input current limit.C
PGOOD7VSSThe PGOOD LED is always on. The incorrect PGOOD status is reported. The charge function is still functional.C
CHG9OUTThere is an increase in the observed input current when the OUT pin is shorted to the CHG pin with VIN present. The charger is still functional. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
OUT11ILIMThe input FET is turned off and charging stops until the short to the OUT pin is removed. The battery powers the output.B
IN13TMRThe device stops charging after the default timer limit is reached. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
TMR14SYSOFFIf the SYSOFF pin is high when shorted to the TMR pin, the device stops charging after the default safety timer duration. If the SYSOFF pin is low when shorted to the TMR pin, the safety timers are disabled.C
SYSOFF15ISETThe ISET pin sets the charge current, so the charge current setting is affected by the SYSOFF pin voltage when these pins are shorted together.C
Table 3-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
TS1The device stops charging in the cold region of the TS pin. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
BAT2The battery and BAT pin are potentially damaged due to an unregulated current path and an exceedance of the absolute maximum rating of the pin. The device resumes charging when the short is removed. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
3
CE4The charging function is disabled. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
EN25The ILIM pin is in either ILIM mode or standby mode. Refer to the EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
EN16The EN1 pin is high. The device is in either USB500 mode or standby mode. Refer to the EN1/EN2 Settings table in the Pin Configuration and Functions section of the datasheet. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
PGOOD7The input current increases. There is no PGOOD indicator function. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
VSS8The input supply is shorted to ground with possible damage to the input if short protection is not present. The current of the system is supplied by the battery but charging does not occur.A
CHG9The input current increases. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
OUT10There is unregulated current from the supply to output. There is pin damage. Downstream devices are potentially damaged. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
11
ILIM12The input FET is turned off and the device stops charging until the short to the supply is removed. The battery powers the output. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
IN13N/AD
TMR14The device stops charging after the default timer limit is reached. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
SYSOFF15The BATFET is off since the SYSOFF pin is high. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A
ISET16The device stops charging. The pin is potentially damaged if fault conditions exceed the absolute maximum ratings in the datasheet for the device.A