SFFSB56 February 2026 DRV81080-Q1 , DRV81242-Q1 , DRV81602-Q1 , DRV81620-Q1
Figure 4-1 shows the DRV81602-Q1 pin diagram for the 24-pin HTSSOP (PWP) package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the DRV81602-Q1 datasheet.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| nSCS | 1 | SPI communication is not functional. | B |
| SCLK | 2 | SPI communication is not functional. | B |
| SDI | 3 | SPI communication is not functional. | B |
| SDO | 4 | SPI communication is not functional. | B |
| GND | 5 | The device operates as intended. | D |
| OUT0_LS | 6 | There is a loss of load control. | B |
| OUT2_D | 7 | There is a loss of load control. | B |
| OUT2_S | 8 | There is a loss of load control. | B |
| OUT4_D | 9 | There is a loss of load control. | B |
| OUT4_S | 10 | There is a loss of load control. | B |
| OUT6_S | 11 | There is a loss of load control. | B |
| OUT6_D | 12 | There is a loss of load control. | B |
| OUT7_D | 13 | There is a loss of load control. | B |
| OUT7_S | 14 | There is a loss of load control. | B |
| OUT5_S | 15 | There is a loss of load control. | B |
| OUT5_D | 16 | There is a loss of load control. | B |
| OUT3_S | 17 | There is a loss of load control. | B |
| OUT3_D | 18 | There is a loss of load control. | B |
| OUT1_LS | 19 | There is a loss of load control. | B |
| VM | 20 | The voltage monitor indicates an undervoltage warning for the supply functions. | B |
| nSLEEP | 21 | SPI communication is not functional. | B |
| IN1 | 22 | There is a loss of load control. | B |
| IN0 | 23 | There is a loss of load control. | B |
| VDD | 24 | SPI communication is not functional. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| nSCS | 1 | SPI communication is not functional. | B |
| SCLK | 2 | SPI communication is not functional. | B |
| SDI | 3 | SPI communication is not functional. | B |
| SDO | 4 | SPI communication is not functional. | B |
| GND | 5 | There is a loss of load control. | B |
| OUT0_LS | 6 | There is a loss of load control. | B |
| OUT2_D | 7 | There is a loss of load control. | B |
| OUT2_S | 8 | There is a loss of load control. | B |
| OUT4_D | 9 | There is a loss of load control. | B |
| OUT4_S | 10 | There is a loss of load control. | B |
| OUT6_S | 11 | There is a loss of load control. | B |
| OUT6_D | 12 | There is a loss of load control. | B |
| OUT7_D | 13 | There is a loss of load control. | B |
| OUT7_S | 14 | There is a loss of load control. | B |
| OUT5_S | 15 | There is a loss of load control. | B |
| OUT5_D | 16 | There is a loss of load control. | B |
| OUT3_S | 17 | There is a loss of load control. | B |
| OUT3_D | 18 | There is a loss of load control. | B |
| OUT1_LS | 19 | There is a loss of load control. | B |
| VM | 20 | The voltage monitor indicates an undervoltage warning for the supply functions. | B |
| nSLEEP | 21 | SPI communication is not functional. | B |
| IN1 | 22 | There is a loss of load control. | B |
| IN0 | 23 | There is a loss of load control. | B |
| VDD | 24 | SPI communication is not functional. | B |
| Pin Name | Pin No. | Shorted to Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| nSCS | 1 | 2 | SPI communication is not functional. | B |
| SCLK | 2 | 3 | SPI communication is not functional. | B |
| SDI | 3 | 4 | SPI communication is not functional. | B |
| SDO | 4 | 5 | SPI communication is not functional. | B |
| GND | 5 | 6 | There is a loss of load control. | B |
| OUT0_LS | 6 | 7 | There is a loss of load control. | B |
| OUT2_D | 7 | 8 | There is a loss of load control. | B |
| OUT2_S | 8 | 9 | There is a loss of load control. | B |
| OUT4_D | 9 | 10 | There is a loss of load control. | B |
| OUT4_S | 10 | 11 | There is a loss of load control. | B |
| OUT6_S | 11 | 12 | There is a loss of load control. | B |
| OUT6_D | 12 | 13 | There is a loss of load control. | B |
| OUT7_D | 13 | 14 | There is a loss of load control. | B |
| OUT7_S | 14 | 15 | There is a loss of load control. | B |
| OUT5_S | 15 | 16 | There is a loss of load control. | B |
| OUT5_D | 16 | 17 | There is a loss of load control. | B |
| OUT3_S | 17 | 18 | There is a loss of load control. | B |
| OUT3_D | 18 | 19 | There is a loss of load control. | B |
| OUT1_LS | 19 | 20 | There is a loss of load control. | B |
| VM | 20 | 21 | False faults are potentially detected on the VM pin. | B |
| nSLEEP | 21 | 22 | There is a loss of load control. | B |
| IN1 | 22 | 23 | There is a loss of load control. | B |
| IN0 | 23 | 24 | There is a loss of load control. | B |
| VDD | 24 | 1 | SPI communication is not functional. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| nSCS | 1 | The maximum voltage of the low voltage pin is violated. | A |
| SCLK | 2 | The maximum voltage of the low voltage pin is violated. | A |
| SDI | 3 | The maximum voltage of the low voltage pin is violated. | A |
| SDO | 4 | The maximum voltage of the low voltage pin is violated. | A |
| GND | 5 | The voltage monitor indicates an undervoltage warning for the supply functions. | B |
| OUT0_LS | 6 | There is a loss of load control. | B |
| OUT2_D | 7 | There is a loss of load control. | B |
| OUT2_S | 8 | There is a loss of load control. | B |
| OUT4_D | 9 | There is a loss of load control. | B |
| OUT4_S | 10 | There is a loss of load control. | B |
| OUT6_S | 11 | There is a loss of load control. | B |
| OUT6_D | 12 | There is a loss of load control. | B |
| OUT7_D | 13 | There is a loss of load control. | B |
| OUT7_S | 14 | There is a loss of load control. | B |
| OUT5_S | 15 | There is a loss of load control. | B |
| OUT5_D | 16 | There is a loss of load control. | B |
| OUT3_S | 17 | There is a loss of load control. | B |
| OUT3_D | 18 | There is a loss of load control. | B |
| OUT1_LS | 19 | There is a loss of load control. | B |
| VM | 20 | The device operates as intended. | D |
| nSLEEP | 21 | There is no impact to the functions of the device. | D |
| IN1 | 22 | The maximum voltage of the low voltage pin is violated. | A |
| IN0 | 23 | The maximum voltage of the low voltage pin is violated. | A |
| VDD | 24 | The maximum voltage of the low voltage pin is violated. | A |