SFFSB09A December   2025  – January 2026 TPSI2240-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPSI2240-Q1, TPSI2240C-Q1, and TPSI2240T-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Note: When the pin short to ground case is discussed, only primary-side ground shorts are considered.
Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the TPSI2240-Q1, TPSI2240C-Q1, and TPSI2240T-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPSI2240-Q1, TPSI2240C-Q1, and TPSI2240T-Q1 datasheets.

TPSI2240-Q1 TPSI2240-Q1, TPSI2240C-Q1, and TPSI2240T-Q1 Pin Diagram Figure 4-1 TPSI2240-Q1, TPSI2240C-Q1, and TPSI2240T-Q1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 The device is in the OFF state (UVLO). The secondary-side switch is in the OFF state. B
GND 2 There is no effect on the device. D
EN 3 The device is in the OFF state. The secondary-side switch is in the OFF state. B
NC/GND 4 There is no effect on the device. D
NC/GND 5 There is no effect on the device. D
NC/GND 6 There is no effect on the device. D
NC/GND 7 There is no effect on the device. D
GND 8 There is no effect on the device. D
S2 9 N/A N/A
NC 10 N/A N/A
S1 11 N/A N/A
Table 4-3 Pin FMA for Device Pins Short-Circuited to VDD
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 There is no effect on the device. D
GND 2 The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. B
EN 3 The device is in the ON state. The secondary side switch is in the ON state. B
NC/GND 4 If pin 3 is high, there is no effect on the device. D
If pin 3 is low, the standoff voltage of the secondary side switch is halved. C
NC/GND 5 If pin 3 is high, there is no effect on the device. D
If pin 3 is low, the standoff voltage of the secondary side switch is halved. C
NC/GND 6 There is no effect on the device. D
NC/GND 7 There is no effect on the device. D
GND 8 The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. B
S2 9 N/A N/A
NC 10 N/A N/A
S1 11 N/A N/A
Table 4-4 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 The device is in the OFF state (UVLO). The secondary-side switch is in the OFF state. B
GND 2 If pin 8 is not connected, the device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. B
EN 3 The device is in the OFF state. The secondary-side switch is in the OFF state. B
NC/GND 4 There is no effect on the device. D
NC/GND 5 There is no effect on the device. D
NC/GND 6 There is no effect on the device. D
NC/GND 7 There is no effect on the device. D
GND 8 If pin 2 is not connected, the device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. B
S2 9 There is no effect on the device. D
NC 10 There is no effect on the device. D
S1 11 There is no effect on the device. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 2 The device is in the OFF state (UVLO). The secondary-side switch is in the OFF state. B
GND 2 3 The device is in the OFF state. The secondary-side switch is in the OFF state. B
EN 3 4 No effect if pin 4 is NC, if pin 4 is GND, the device is in the OFF state, and the secondary-side switch is in the OFF state. D
B
NC/GND 4 5 There is no effect on the device. D
NC/GND 5 6 There is no effect on the device. D
NC/GND 6 7 There is no effect on the device. D
NC/GND 7 8 There is no effect on the device. D
GND 8 9 N/A N/A
S2 9 10 There is no effect on the device. D
NC 10 11 There is no effect on the device. D
S1 11 1 N/A N/A