SFFSAY5 February 2026 UCC34141-Q1
Figure 4-1 shows the UCC34141-Q1 pin diagram for the DHA-16 package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the UCC34141-Q1 datasheet.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| ENA | 1 | The device is disabled. There is no output. | B |
| PG (PG) | 2 | The power good signal is always low. The MCU cannot detect the status of the bias supply. | C |
| VIN | 3 | The device is not powered. There is no output. | B |
| VIN | 4 | The device is not powered. There is no output. | B |
| GNDP | 5 | There is no effect on the device. | D |
| GNDP | 6 | There is no effect on the device. | D |
| GNDP | 7 | There is no effect on the device. | D |
| GNDP | 8 | There is no effect on the device. | D |
| COMA | 9 | There is no effect on the device. | D |
| COM | 10 | There is no effect on the device. | D |
| COM | 11 | There is no effect on the device. | D |
| VDD | 12 | The device is disabled. There is no output. | B |
| BSW | 13 | The device is disabled. There is no output. | B |
| VEE | 14 | The device is disabled. There is no output. | B |
| FBVDD | 15 | The device is disabled. There is no output. | B |
| FBVEE | 16 | The device is disabled. There is no output. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| ENA | 1 | The state of the device is undetermined. The device can be on or off, depending on the noise on ENA pin. | B |
| PG (PG) | 2 | The MCU cannot detect the status of the bias supply. | C |
| VIN | 3 | There is no effect on the device. | D |
| VIN | 4 | There is no effect on the device. | D |
| GNDP | 5 | There is no effect on the device. | D |
| GNDP | 6 | There is no effect on the device. | D |
| GNDP | 7 | There is no effect on the device. | D |
| GNDP | 8 | There is no effect on the device. | D |
| COMA | 9 | The feedback reference voltage and the VDD regulation voltage have offset. | B |
| COM | 10 | There is no effect on the device. | D |
| COM | 11 | The power stage current goes through the internal diode. There is more noise on the feedback signals. | C |
| VDD | 12 | The device is disabled. There is no output. | B |
| BSW | 13 | The device is disabled. There is no output. | B |
| VEE | 14 | The device is disabled. There is no output. | B |
| FBVDD | 15 | The device is disabled. There is no output. | B |
| FBVEE | 16 | The device is disabled. There is no output. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| ENA | 1 | PG (PG) | The device is disabled. There is no output. | B |
| PG (PG) | 2 | VIN | The absolute maximum rating is exceeded for the pin. Damage to the device is possible. | A |
| VIN | 3 | VIN | There is no effect on the device. | D |
| VIN | 4 | GNDP | The device is not powered. There is no output. | B |
| GNDP | 5 | GNDP | There is no effect on the device. | D |
| GNDP | 6 | GNDP | There is no effect on the device. | D |
| GNDP | 7 | GNDP | There is no effect on the device. | D |
| GNDP | 8 | N/A | N/A | N/A |
| COMA | 9 | COM | There is no effect on the device. | D |
| COM | 10 | COM | There is no effect on the device. | D |
| COM | 11 | VDD | The device is disabled. There is no output. | B |
| VDD | 12 | BSW | The device is disabled. There is no output. | B |
| BSW | 13 | VEE | The device is disabled. There is no output. | B |
| VEE | 14 | FBVDD | The device is disabled. There is no output. | B |
| FBVDD | 15 | FBVEE | The device is disabled. There is no output. | B |
| FBVEE | 16 | N/A | N/A | N/A |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| ENA | 1 | The absolute maximum rating is exceeded for the pin. Damage to the device is possible. | A |
| PG (PG) | 2 | The absolute maximum rating is exceeded for the pin. Damage to the device is possible. | A |
| VIN | 3 | There is no effect on the device. | D |
| VIN | 4 | There is no effect on the device. | D |
| GNDP | 5 | The device is not powered. There is no output. | B |
| GNDP | 6 | The device is not powered. There is no output. | B |
| GNDP | 7 | The device is not powered. There is no output. | B |
| GNDP | 8 | The device is not powered. There is no output. | B |
| COMA | 9 | The device is not powered. There is no output. | B |
| COM | 10 | The device is disabled. There is no output. | B |
| COM | 11 | The device is disabled. There is no output. | B |
| VDD | 12 | There is no effect on the device. | D |
| BSW | 13 | The device is disabled. There is no output. | B |
| VEE | 14 | The device is disabled. There is no output. | B |
| FBVDD | 15 | The device is disabled. There is no output. | B |
| FBVEE | 16 | The absolute maximum rating is exceeded for the pin. Damage to the device is possible. | A |