SFFSAW0A December 2025 – December 2025 TPSI2260-Q1
This section provides a failure mode analysis (FMA) for the pins of the TPSI2260-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Below is the TPSI2260-Q1 pin diagram package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPSI2260-Q1 data sheet.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VDD | 1 | The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. | B |
| GND | 2 | There is no effect on the device. | D |
| EN | 3 | The device is in the OFF state, the secondary-side switch is in the OFF state. | B |
| NC/GND | 4 | There is no effect on the device. | D |
| NC/GND | 5 | There is no effect on the device. | D |
| NC/GND | 6 | There is no effect on the device. | D |
| NC/GND | 7 | There is no effect on the device. | D |
| GND | 8 | There is no effect on the device. | D |
| S2 | 9 | N/A | N/A |
| SM | 10 | N/A | N/A |
| S1 | 11 | N/A | N/A |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VDD | 1 | There is no effect on the device. | D |
| GND | 2 | The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. | B |
| EN | 3 | The device is in the ON state, the secondary-side switch is in the ON state. | B |
| NC/GND | 4 | There is no effect on the device. | D |
| NC/GND | 5 | There is no effect on the device. | D |
| NC/GND | 6 | There is no effect on the device. | D |
| NC/GND | 7 | There is no effect on the device. | D |
| GND | 8 | The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. | B |
| S2 | 9 | N/A | N/A |
| SM | 10 | N/A | N/A |
| S1 | 11 | N/A | N/A |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| VDD | 1 | The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. | B |
| GND | 2 | The device is in the OFF state, the secondary-side switch is in the OFF state. | D |
| EN | 3 | The device is in the OFF state, the secondary-side switch is in the OFF state. | B |
| NC/GND | 4 | There is no effect on the device. | D |
| NC/GND | 5 | There is no effect on the device. | D |
| NC/GND | 6 | There is no effect on the device. | D |
| NC/GND | 7 | There is no effect on the device. | D |
| GND | 8 | There is no effect on the device. | D |
| S2 | 9 | There is no effect on the device. | D |
| SM | 10 | There is no effect on the device. | D |
| S1 | 11 | There is no effect on the device. | D |
| Pin Name | Pin No. | Shorted to Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| VDD | 1 | 2 | The device is in the OFF state (UVLO), the secondary-side switch is in the OFF state. | B |
| GND | 2 | 3 | There is no effect on the device. | B |
| EN | 3 | 4 | No effect if pin 4 is NC, if pin 4 is GND the device is in the OFF state, the secondary-side switch is in the OFF state. | D |
| B | ||||
| NC/GND | 4 | 5 | There is no effect on the device. | D |
| NC/GND | 5 | 6 | There is no effect on the device. | D |
| NC/GND | 6 | 7 | There is no effect on the device. | D |
| NC/GND | 7 | 8 | There is no effect on the device. | D |
| GND | 8 | 9 | N/A | N/A |
| S2 | 9 | 10 | The device is only capable of blocking positive voltage from the S1 to S2 pins when the switches are OFF. | C |
| SM | 10 | 11 | The device is only capable of blocking negative voltage from the S1 to S2 pins when the switches are OFF. | C |
| S1 | 11 | 1 | N/A | N/A |