SFFSAG0 June   2025 TPS22950-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS22950-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the TPS22950-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS22950-Q1 data sheet.

TPS22950-Q1 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device pins are connected per the recommendation in the data sheet, including pullup and pulldown resistors, as needed.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
ON 1 The device turns off. B
VIN 2 The power supply is shorted. D
GND 3 This is the intended operation for the GND pin. D
ILIM 4 The current limit block does not limit the current. A
VOUT 5 If the current limit is set, the device tries to limit the current to a value set by ILIM. B
FLT 6 Grounding this pin does not allow the device to indicate the fault properly. C
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
ON 1 The device is off. The device does not pass through voltage to VOUT. B
VIN 2 No power supply to the device. The device does not pass through voltage to VOUT. D
GND 3 No ground to the device. The device does not function. D
ILIM 4 The current limit block does not function correctly. B
VOUT 5 The output does not deliver the voltage to the load. D
FLT 6 There is no pullup to read the Fault pin status. D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
ON 1 VIN The device is enabled if the VIN power supply is above the ON threshold (VIH). D
VIN 2 GND The device does not have power supply. D
ILIM 4 VOUT Incorrect current limit function. The device potentially turns off and on since the current limit threshold depends on the voltage of the VOUT pin. B
VOUT 5 FLT No effect during no fault. During a fault condition, the Fault pin can conduct large amounts of current from VOUT to GND. A
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
ON 1 Normal operation is expected. D
VIN 2 Normal operation is expected. D
GND 3 The power supply is shorted. D
ILIM 4 The device does not turn on. B
VOUT 5 The power MOSFET is shorted. Disabling the device no longer blocks power to VOUT. B
FLT 6 During a fault condition, the Fault pin draws huge amounts of current; potentially damaging the pin. A