SFFSAD7 June   2025 TPS4HC120-Q1

PRODUCTION DATA  

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS4HC120-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the TPS4HC120-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS4HC120-Q1 data sheet.

Figure 4-1 Pin Diagram

Following is the of use and the device configuration assumed for the pin FMA in this section:

  • The device is used with external components consistent with the values described in the external component table of the data sheet.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
NC1No effect.D
EN12The corresponding channel shuts down.B
EN23The corresponding channel shuts down.B
EN34The corresponding channel shuts down.B
EN45The corresponding channel shuts down.B
SEL16The sense function is activated for only channel 1 or 3.B
SEL07The sense function is activated for only channel 1 or 2.B
DIAG_EN8The diagnostics are disabled.B
FLT_9The status reported is potentially erroneous.B
LPM10The LPM status reported is potentially erroneous.B
SNS11The sense current is not valid from the SNS pin.B
ILIM12The device defaults to 2.25A current limit.C
GND13The resistor or diode network is bypassed, if present.B
NC14No effect.D
VOUT415The current limit of the device engages.B
VOUT416The current limit of the device engages.B
VOUT317The current limit of the device engages.B
VOUT318The current limit of the device engages.B
NC19No effect.D
VBB20The device has no input supply, and therefore, does not function.B
VBB21The device has no input supply, and therefore, does not function.B
VBB22The device has no input supply, and therefore, does not function.B
VBB23The device has no input supply, and therefore, does not function.B
NC24No effect.D
VOUT225The current limit of the device engages.B
VOUT226The current limit of the device engages.B
VOUT127The current limit of the device engages.B
VOUT128The current limit of the device engages.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
NC1No effect.D
EN12Channel 1 shuts down, EN is pulled down internally.B
EN23Channel 2 shuts down, EN is pulled down internally.B
EN34Channel 3 shuts down, EN is pulled down internally.B
EN45Channel 4 shuts down, EN is pulled down internally.B
SEL16Internally pulled down. The sense function is activated for only channel 1 or 3B
SEL07Internally pulled down. The sense function is activated for only channel 1 or 2.B
DIAG_EN8Internally pulled down. The diagnostics are disabled.B
FLT_9The fault signal is not reported.B
LPM10The LPM signal is not reported.B
SNS11The correct sense current cannot be read.B
ILIM12The device defaults to 5A current limit.C
GND13Loss of ground detection engages and the device shuts off.B
NC14No effect.D
VOUT415No effect. If configured, open-load detection triggers.B
VOUT416No effect. If configured, open-load detection triggers.B
VOUT317No effect. If configured, open-load detection triggers.B
VOUT318No effect. If configured, open-load detection triggers.B
NC19No effect.D
VBB20The device has no input supply, and therefore, does not function.B
VBB21The device has no input supply, and therefore, does not function.B
VBB22The device has no input supply, and therefore, does not function.B
VBB23The device has no input supply, and therefore, does not function.B
NC24No effect.D
VOUT225No effect. If configured, open-load detection triggers.B
VOUT226No effect. If configured, open-load detection triggers.B
VOUT127No effect. If configured, open-load detection triggers.B
VOUT128No effect. If configured, open-load detection triggers.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted to Pin No.Description of Potential Failure EffectsFailure Effect Class
NC12No effect.D
EN123The EN1 signal affects the EN2 signal, and the EN2 signal affects the EN1 signal.B
EN234The EN2 signal affects the EN3 signal, and the EN3 signal affects the EN2 signal.B
EN345The EN3 signal affects the EN4 signal, and the EN4 signal affects the EN3 signal.B
EN456The EN4 signal affects the SEL1 signal, and the SEL1 signal affects the EN4 signal.B
SEL167The SEL1 signal affects the SEL0 signal, and the SEL0 signal affects the SEL1 signal.B
SEL078The SEL0 signal affects the DIAG_EN signal, and the DIAG_EN signal affects the SEL0 signal.B
DIAG_EN89Fault reporting is erroneous, diagnostics are enabled if the FLT_ pin is high.B
FLT_910The reports of Fault and LPM are potentially erroneous.B
LPM1011The reports of current sensing and LPM are potentially erroneous.B
SNS1112The outputs of current limit and current sensing are incorrect.B
ILIM1213The device defaults to 2.25A current limit.B
GND1314No effect.D
VOUT41516No effect.D
VOUT41617There is a potential loss of load control on channels 3 and 4.B
VOUT31718No effect.D
VOUT31819No effect.D
NC1920No effect.D
VBB2021No effect.D
VBB2122No effect.D
VBB2223No effect.D
VBB2324No effect.D
NC2425No effect.D
VOUT22526No effect.D
VOUT22627There is a potential loss of load control on channels 1 and 2.B
VOUT12728No effect.D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
NC1No effect.D
EN12There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
EN23There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
EN34There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
EN45There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
SEL16There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
SEL07There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
DIAG_EN8There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
FLT_9There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
LPM10There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
SNS11There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
ILIM12There is a violation of the absolute maximum rating of the pin.
A breakdown of the ESD cell is possible.
A
GND13The supply power is bypassed and the device does not turn on.B
NC14No effect.D
VOUT415The output is pulled to supply; a short-to-battery triggers, if configured.D
VOUT416The output is pulled to supply; a short-to-battery triggers, if configured.B
VOUT317The output is pulled to supply; a short-to-battery triggers, if configured.B
VOUT318The output is pulled to supply; a short-to-battery triggers, if configured.B
NC19No effect.D
VBB20Intended operation.D
VBB21Intended operation.D
VBB22Intended operation.D
VBB23Intended operation.D
NC24No effect.D
VOUT225The output is pulled to supply; a short-to-battery triggers, if configured.B
VOUT226The output is pulled to supply; a short-to-battery triggers, if configured.B
VOUT127The output is pulled to supply; a short-to-battery triggers, if configured.B
VOUT128The output is pulled to supply; a short-to-battery triggers, if configured.B