SFFSAD5 July 2025 TPS7B87-Q1
Figure 4-2 shows the TPS7B87-Q1 pin diagram for the HSOIC package B version with PG. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS7B87-Q1 data sheet.
Figure 4-2 Pin Diagram | Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| OUT | 1 | Regulation is not possible, the device operates at current limit. The device can cycle in and out of thermal shutdown. | B |
| NC | 2 | No effect. Normal operation. | B |
| DELAY | 3 | Ground current is permanently increased. | C |
| NC | 4 | No effect. Normal operation. | D |
| GND | 5 | No effect. Normal operation. | D |
| PG | 6 | Power-good never asserts when the output voltage is at target, thus, potentially effecting power sequencing. | B |
| NC | 7 | No effect. Normal operation. | D |
| IN | 8 | Power is not supplied to the device. System performance depends on upstream current limiting. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| OUT | 1 | The device output is disconnected from the load. | B |
| NC | 2 | No effect. Normal operation. | D |
| DELAY | 3 | The power-good delay is set to the minimum delay time, t(DLY_FIX). | C |
| NC | 4 | No effect. Normal operation. | D |
| GND | 5 | There is no current loop for the supply voltage. The device is not operational and does not regulate. | B |
| PG | 6 | The power-good signal is not accessible. Power sequencing can be effected. | B |
| NC | 7 | No effect. Normal operation. | D |
| IN | 8 | Power is not supplied to the device, resulting in no output voltage. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| OUT | 1 | 2 - NC | No effect. Normal operation. | D |
| NC | 2 | 3 - DELAY | No effect. Normal operation. | D |
| DELAY | 3 | 4 - NC | No effect. Normal operation. | D |
| GND | 5 | 6 - PG | Power-good functionality cannot operate correctly, always low. | B |
| PG | 6 | 7 - NC | No effect. Normal operation. | D |
| NC | 7 | 8 - IN | No effect. Normal operation. | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| OUT | 1 | Output held at VIN, regulation is not possible. Damage is possible if the absolute maximum rating is exceeded (20V max). | A |
| NC | 2 | No effect. Normal operation. | D |
| DELAY | 3 | PG can incorrectly assert when the output voltage is not at target. The pin absolute maximum rating (6V max) can be exceeded and the pin can be damaged. | A |
| B | |||
| NC | 4 | No effect. Normal operation. | D |
| GND | 5 | Power is not supplied to the device. System performance depends on upstream current limiting. | B |
| PG | 6 | Power-good functionality cannot operate correctly. PG can be damaged if the absolute maximum rating (20V) is violated. | A |
| B | |||
| NC | 7 | No effect. Normal operation. | D |
| IN | 8 | No effect. Normal operation. | D |