SFFSA21 October   2025 LM25190-Q1 , LM5190-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the LM5190-Q1 and LM25190-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the LM5190-Q1 and LM25190-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LM5190-Q1 and LM25190-Q1 datasheets.

LMx5190-Q1 LM5190-Q1 LM25190-Q1 Pin Diagram Figure 4-1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
ISET1VOUT = 0V. The ISET pin is not functional.B
RT2The output voltage attempts to regulate at maximum FSW, causing maximum power dissipation.C
COMP3VOUT = 0V.B
FB4The target of the output voltage is set to 5V.B
AGND5The AGND pin is GND. VOUT = VOUT is as expected.D
IMON/ILIM6VOUT = VOUT is as expected. The current monitor and CC limit are not functional.B
VCC7VOUT = 0V, the device does not switch, the output of the VCC pin is loaded.B
PGND8The PGND pin is GND. VOUT = VOUT is as expected.D
LO9VOUT = 0V, the internal VCC regulator is loaded to current limit.B
VIN10VOUT = 0V.B
HO11VOUT = 0V, the internal VCC regulator is loaded to current limit.B
SW12VOUT = 0V. The high-side FET is shorted from the VIN pin to GND.A
CBOOT13VOUT = 0V. The high-side FET is shorted from the VIN pin to GND.B
BIAS14VOUT = VOUT is as expected. The internal VCC regulator provides bias voltage.C
PGOOD15VOUT = VOUT is as expected. The PGOOD pin is not functional.C
FPWM/SYNC16VOUT = VOUT is as expected. There is no synchronization available and the device is always in PFM mode.C
EN17VOUT = 0V. The device is always in shutdown.B
ISNS+18VOUT = 0V.A
VOUT19VOUT = 0V.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
ISET 1 VOUT = VOUT is as expected. The ISET pin is not functional. C
RT 2 The RT pin regulates to 1V, but the internal oscillator does not function. B
COMP 3 The output voltage oscillates. A
FB 4 VOUT = VIN. A
AGND 5 The output voltage is indeterminate. B
IMON/ILIM 6 VOUT = 0V. The current monitor and CC limit are not functional. B
VCC 7 VOUT = 0V. B
PGND 8 VOUT = 0V. B
LO 9 VOUT = VOUT is as expected but with reduced efficiency. C
VIN 10 VOUT = 0V. B
HO 11 If the HO pin is opened while the HO pin has voltage to the SW pin, the high-side FET never turns off. VOUT = VIN. A
SW 12 The output voltage is indeterminate. The floating rail of the CBOOT pin has no reference to the actual node of the SW pin. VOUT = VIN. A
CBOOT 13 VOUT = 0V. B
BIAS 14 VOUT = VOUT is as expected. The internal VCC regulator provides bias voltage. C
PGOOD 15 VOUT = VOUT is as expected. The PGOOD pin is not functional. C
FPWM/SYNC 16 VOUT = VOUT is as expected. There is no synchronization available and the device is always in FPWM mode. C
EN 17 VOUT = 0V. B
ISNS+ 18 The open ISNS+ pin blocks current limit and causes the output voltage to oscillate. A
VOUT 19 VOUT = 0V, if the internal feedback is used. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
ISET 1 RT

If the resistor of the RT pin is tied to the VCC pin, the ISET pin can be damaged.

If the resistor of the RT pin is tied to the AGND pin, VOUT = VOUT is as expected. The switching frequency is lower. The CC operation is affected.

A
RT 2 COMP

If the resistor of the RT pin is tied to the VCC pin, the COMP pin can be damaged.

If the resistor of the RT pin is tied to the AGND pin, VOUT = 0V.

A
COMP 3 FB External FB mode: The COMP pin regulates to 0.8V and the output is unregulated. VOUT = indeterminate. B
Internal FB mode FB = VCC, there is damage to the device. A
Internal FB mode FB = GND, VOUT = 0V. B
FB 4 AGND The target of the output voltage is set to 5V. B
AGND 5 IMON/ILIM VOUT = VOUT is as expected. The current monitor and CC limit are not functional. C
IMON/ILIM 6 VCC There is damage to the device. A
VCC 7 PGND The VCC pin is grounded. VOUT = 0V. B
PGND 8 LO VOUT = 0V. The VCC pin is loaded by the LO driver. B
LO 9 VIN VOUT = 0V. The driver is damaged if VIN > 8V. A
VIN 10 HO

For VIN > 8V, the pin exceeds the maximum ratings and the HO pin is damaged.

For VIN < 8V, VOUT = dropout is lower than the VIN pin voltage, no switching, and there is excess current from the VIN pin.

A
HO 11 SW VOUT = 0V. B
SW 12 CBOOT VOUT = 0V. B
CBOOT 13 BIAS There is damage to the device if CBOOT > 30V. A
BIAS 14 PGOOD The pulldown of the PG pin can be damaged. VOUT = VOUT is as expected. A
PGOOD 15 FPWM/SYNC

VOUT = VOUT is as expected.

If the FPWM pin is tied to the VCC pin, the pulldown of the PG pin can be damaged.

A
FPWM/SYNC 16 EN VOUT = VOUT is as expected. A
EN 17 ISNS+ The EN pin is high-voltage rated. VOUT = VOUT is as expected if VOUT > 1V. If VOUT < 1V, the device is disabled. B
ISNS+ 18 VOUT

The current limit is disabled since the current limit resistor is shorted.

The output voltage cannot regulate since current-mode feedback is shorted.

A
VOUT 19 ISET

VOUT = 0V.

If prebias VOUT > 5.5V, the ISET pin is damaged.

A
Table 4-5 Pin FMA for Device Pins Short-Circuited to VIN
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
ISET 1 There is damage to the device if VIN > 5.5V. A
RT 2 There is damage to the device if VIN > 8V. A
COMP 3

There is damage to the device if VIN > 5.5V

If VIN < 5.5V, the output voltage is out of regulation.

A
FB 4

There is damage to the device if VIN > 8V.

If VIN < 8V, VOUT = VIN is as expected.

A
AGND 5 VOUT = 0V. B
IMON/ILIM 6 There is damage to the device if VIN > 5.5V. A
VCC 7

There is damage to the device if VIN > 8V.

If VIN < 8V, VOUT = VOUT is as expected.

A
PGND 8 VOUT = 0V. B
LO 9 VOUT = 0V. The driver is damaged if VIN > 8V. A
VIN 10 N/A D
HO 11

For VIN > 8V, the pin exceeds the maximum ratings and the HO pin is damaged.

For VIN < 8V, VOUT = dropout is lower than the VIN pin, there is no switching, and there is excess current from the VIN pin.

A
SW 12 VOUT = VIN, there is excess current from the VIN pin. The LO pin turns on and shorts against the VIN pin. B
CBOOT 13

There is damage to the device if VIN > 8V.

If VIN < 8V, VOUT < the output voltage target.

A
BIAS 14 There is damage to the device if VIN > 30V. A
PGOOD 15 There is damage to the device. A
FPWM/SYNC 16

There is damage to the device if VIN > 8V.

If VIN < 8V, VOUT = VOUT is as expected, but the device is always in FPWM mode.

A
EN 17 The device is always on. VOUT = VOUT is as expected. C
ISNS+ 18 There is damage to the device. A
VOUT 19 VOUT = VIN. B