SFFS988 September   2024 LM5109B-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the LM5109B-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality.
B No device damage, but loss of functionality.
C No device damage, but performance degradation.
D No device damage, no impact to functionality or performance.

Figure 4-1 shows the LM5109B-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the LM5109B-Q1 data sheet.

LM5109B-Q1 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Short between VDD and HB is not considered.
  • Short between VSS and LO is not considered.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 The device is not powered. C
HI 2 HO is pulled low (sinking is on). HI is stuck low. C
LI 3 LO is pulled low (sinking is on). LI is stuck low. C
VSS 4 No impact. Short to same potential. D
LO 5 LO is stuck low. A
HS 6 HS is stuck low. Power FET short circuit HV and HS when HI = H is commanded. D
HO 7 HO is stuck low. Device damage is possible when HI = H is commanded. A
HB 8 HO is stuck low. Boot diode damage is possible. D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 The device is not powered. D
HI 2 HI is pulled down by the internal pulldown resistor. HO is pulled down (sinking is on). C
LI 3 LI is pulled down by the internal pulldown resistor. LO is pulled down (sinking is on). C
VSS 4 HI and LI float to VDD level. HO and LO float to VDD level. C
LO 5 LO is disconnected from the gate of the power FET. D
HS 6 Low side output has no supply. LO is pulled down (sinking is on). C
HO 7 HO is disconnected from the gate of the power FET. D
HB 8 High-side output has no supply. HO is pulled down (sinking is on). C
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
VDD 1 HI HI is stuck high. HO is pulled up (sourcing is on). C
HI 2 LI HI and LI are undefined. C
LI 3 VSS LI is stuck low. C
VSS 4 N/A N/A N/A
LO 5 HS LO is in an overvoltage condition and potentially exposed to VIN level when HI = H is commanded. A
HS 6 HO High-side HO output level is 0 (HO-HS). High-side power FET is off (VGS is stuck low). A
HO 7 HB HO is stuck high. HO is pulled up to VDD level. Power FET damage is possible when LI = H is commanded. A
HB 8 N/A N/A N/A
Table 4-5 Pin FMA for Device Pins Short-Circuited to VDD
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VDD 1 No impact. Short to same potential. D
HI 2 HI is stuck high. HO is pulled up (sourcing is on). C
LI 3 LI is stuck high. LO is pulled up (sourcing is on). C
VSS 4 VDD short to VSS The device is not powered. C
LO 5 LO is stuck high and device damage is possible. Power FET damage is possible when HI = H is commanded. A
HS 6 HO (and HS) is pulled to VDD level. C
HO 7 HO is stuck high and device damage is possible. Power FET damage is possible when LI = H is commanded. A
HB 8 HO output voltage (sourcing on) is lower than the specified range. C