SFFS791 February   2024 TXU0101-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 SC70 Package
    2. 2.2 SON Package
    3. 2.3 SC70 and SON Packages
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TXU0101-Q1 (SC70 and SON packages). The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

Figure 4-1 and Figure 4-2 shows the TXU0101-Q1 pin diagram for the SC70 and SON packages. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TXU0101-Q1 data sheet.

Figure 4-1 Pin Diagram (SC70) Package
Figure 4-2 Pin Diagram (SON) Package
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Device will not be powered or damaged, because short is external to device. System level damage can occur in this scenario.B
GND2Normal operation.D
A3A will be LOW, if corresponding B is HIGH, there will be potential damage to the device if the current is not limited. If corresponding B is LOW, then nothing will occur; there is no damage.B
BY4B will be LOW, if corresponding A is HIGH, there will be potential damage to the device if the current is not limited. If corresponding A is LOW, then nothing will occur; there is no damage.B
OE5All I/Os will be fixed into high impedance (tri-state).B
VCCB6Device will not be powered or damaged, because short is external to device. System level damage may occur in this scenario.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA 1 Device will not be powered. B
GND 2 Device will not be powered. B
A3A pin will be grounded internally.D
BY4B pin will be in HiZ if device is disabled. If device is enabled, it will be high or LOW depending on the input.D
OE 5 All I/Os will be fixed into high impedance (tri-state). A
VCCB6Device will not be powered.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VCCA 1 GND Device will not be powered or damaged, because short is external to device. System level damage may occur in this scenario. B
GND 2 A A will be LOW, if corresponding B is HIGH, there will be potential damage to the device if the current is not limited. If corresponding B is LOW, then nothing will occur, no damage. B
A3BYOne input on VCCA supply is shorted to one output of VCCB supply. Based on the external bus driving this connection, potential high current can be expected if the VILA is less than Input Voltage A is less than VIHA or if BY output gets an undeterministic voltage forced on it in presence of a valid input.A
BY4OEB pin will in HiZ if device is disabled. If device is enabled, it will be HIGH or LOW depending upon the input.D
OE 5 VCCB All I/Os will be active, device cannot be disabled. B
VCCB6VCCADevice will not be powered or damaged, because short is external to device. System level damage may occur in this scenario.B
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply (VCCA)
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA 1 Normal operation. D
GND 2 Device will not be powered or damaged, because short is external to device. System level damage may occur in this scenario. B
A3Ax will be HIGH, if corresponding Bx is LOW, there will be potential damage to the device if the current is not limited. If corresponding Bx is HIGH, then nothing will occur, no damage.B
BY4Bx will be HIGH, if corresponding Ax is LOW, there will be potential damage to the device if the current is not limited. If corresponding Ax is HIGH, then nothing will occur; there is no damage.B
OE 5 All I/Os will be active, device cannot be disabled. B
VCCB6Device will not be powered or damaged, because short is external to device. System level damage may occur in this scenario.B
Table 4-6 Pin FMA for Device Pins Short-Circuited to supply VCCB
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA 1 Device will not be powered or damaged, because short is external to device. System level damage may occur in this scenario. B
GND 2 Device will not be powered or damaged, because short is external to device. System level damage may occur in this scenario. B
A3Ax will be HIGH, if corresponding Bx is HIGH, there will be potential damage to the device if the current is not limited. If corresponding Bx is HIGH, then nothing will occur; there is no damage.B
BY4Bx will be HIGH, if corresponding Ax is LOW, there will be potential damage to the device if the current is not limited. If corresponding Ax is HIGH, then nothing will occur; there is no damage.B
OE 5 All I/Os will be active, device cannot be disabled. B
VCCB6Normal operation.D