SFFS658 july 2023 DAC539G2-Q1
This section provides a failure mode analysis (FMA) for the pins of the DAC539G2-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the DAC539G2-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the DAC539G2-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| FB0 | 1 | OUT0 (PWM) is always high | B |
| OUT0 | 2 | OUT0 is be stuck at zero if OUT0 is configured as open drain | B |
| Device can be damaged over a period of time if OUT0 is configured in push-pull mode | A | ||
| NC | 3 | No change in functionality or performance | D |
| NC | 4 | No change in functionality or performance | D |
| SDO | 5 | Read back data is corrupted | B |
| SCL/SYNC/GPI2 | 6 | Loss of communication with the device | B |
| A0/SDI/GPI1 | 7 | Loss of communication with the device | B |
| SDA/SCLK/GPI0 | 8 | Loss of communication with the device | B |
| NC | 9 | No change in functionality or performance | D |
| NC | 10 | No change in functionality or performance | D |
| OUT1 | 11 | OUT0 (PWM) is always high, resulting in incorrect PWM duty cycle | B |
| FB1 | 12 | OUT0 (PWM) is always high, resulting in incorrect PWM duty cycle | B |
| CAP | 13 | Loss of functionality, device enters short circuit protection, power consumption increases | B |
| AGND | 14 | No change in functionality or performance | D |
| VDD | 15 | Complete loss of functionality, no device damage | B |
| MODE | 16 | Loss of GPI functionality | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| FB0 | 1 | OUT0 (PWM) results in incorrect duty cycle | B |
| OUT0 | 2 | OUT0 output value is not available | B |
| NC | 3 | No change in functionality or performance | D |
| NC | 4 | No change in functionality or performance | D |
| SDO | 5 | Read back data is not available | B |
| SCL/SYNC/GPI2 | 6 | Loss of communication with the device | B |
| A0/SDI/GPI1 | 7 | Loss of communication with the device | B |
| SDA/SCLK/GPI0 | 8 | Loss of communication with the device | B |
| NC | 9 | No change in functionality or performance | D |
| NC | 10 | No change in functionality or performance | D |
| OUT1 | 11 | OUT0 (PWM) will result in incorrect duty cycle | B |
| FB1 | 12 | OUT0 (PWM) will result in incorrect duty cycle | B |
| CAP | 13 | Open-circuited pin can cause damage to the low-voltage digital core and NVM supplied by the internal LDO | A |
| AGND | 14 | Complete loss of functionality, no device damage | B |
| VDD | 15 | Complete loss of functionality, no device damage | B |
| MODE | 16 | Loss of communication and GPI functionality | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| FB0 | 1 | MODE | Short to corner pin is not expected | D |
| OUT0 | OUT0 (PWM) results in incorrect duty cycle | B | ||
| OUT0 | 2 | FB0 | OUT0 (PWM) results in incorrect duty cycle | B |
| NC | No change in functionality or performance | D | ||
| NC | 3 | OUT0 | No change in functionality or performance | D |
| NC | No change in functionality or performance | D | ||
| NC | 4 | NC | No change in functionality or performance | D |
| SDO | Short to corner pin is not expected | D | ||
| SDO | 5 | NC | Short to corner pin is not expected | D |
| SCL/SYNC/GPI2 | Loss of communication,GPI and SDO functionality | B | ||
| SCL/SYNC/GPI2 | 6 | SDO | Loss of communication, GPI and SDO functionality | B |
| A0/SDI/GPI1 | Loss of communication and GPI functionality | B | ||
| A0/SDI/GPI1 | 7 | SCL/SYNC/GPI2 | Loss of communication and GPI functionality | B |
| SDA/SCLK/GPI0 | Loss of communication and GPI functionality | B | ||
| SDA/SCLK/GPI0 | 8 | A0/SDI/GPI1 | Loss of communication and GPI functionality | B |
| NC | Short to corner pin is not expected | D | ||
| NC | 9 | SDA/SCLK/GPI0 | Short to corner pin is not expected | D |
| NC | No change in functionality or performance | D | ||
| NC | 10 | NC | No change in functionality or performance | D |
| OUT1 | No change in functionality or performance | D | ||
| OUT1 | 11 | NC | No change in functionality or performance | D |
| FB1 | This is intended connection | D | ||
| FB1 | 12 | OUT1 | This is intended connection | D |
| CAP | Short to corner pin is not expected | D | ||
| CAP | 13 | FB1 | Short to corner pin is not expected | D |
| AGND | Device enters short circuit protection, power consumption increases | B | ||
| AGND | 14 | CAP | Device enters short circuit protection, power consumption increases | B |
| VDD | Complete loss of functionality, no device damage | B | ||
| VDD | 15 | AGND | Complete loss of functionality, no device damage | B |
| MODE | Loss of communication functionality | B | ||
| MODE | 16 | VDD | Loss of communication functionality | B |
| FB0 | Short to corner pin is not expected | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| FB0 | 1 | OUT0 (PWM) is always low | B |
| OUT0 | 2 | Device can be damaged over a period of time | A |
| NC | 3 | No change in functionality or performance | D |
| NC | 4 | No change in functionality or performance | D |
| SDO | 5 | Read back data is corrupted | B |
| SCL/SYNC/GPI2 | 6 | Loss of communication with the device | B |
| A0/SDI/GPI1 | 7 | Loss of communication with the device | B |
| SDA/SCLK/GPI0 | 8 | Loss of communication with the device | B |
| NC | 9 | No change in functionality or performance | D |
| NC | 10 | No change in functionality or performance | D |
| OUT1 | 11 | OUT0 (PWM) is always low | B |
| FB1 | 12 | OUT0 (PWM) is always low | B |
| CAP | 13 | Open-circuited pin can cause damage to the low-voltage digital core and NVM supplied by the internal LDO | A |
| AGND | 14 | Complete loss of functionality, no device damage | B |
| VDD | 15 | No change in functionality or performance | D |
| MODE | 16 | Loss of communication functionality | B |