SFFS627 may 2023 INA310A-Q1 , INA310B-Q1
PRODUCTION DATA
This section provides a Failure Mode Analysis (FMA) for the pins of the INA310-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality |
| B | No device damage, but loss of functionality |
| C | No device damage, but performance degradation |
| D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the INA310-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the INA310-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| VS | 1 | Power supply shorted to ground. | B |
| OUT | 2 | Output shorts to ground. When left in this configuration for a long time, under high supplies self heating could cause dice junction temperature to exceed 150 degrees Celsius. | B |
| CMPIN | 3 | Comparator output is stuck low. | B |
| GND | 4 | Normal operation. | D |
| RESET | 5 | Comparator is in Transparant Mode. If intended connection is not GND or open, functionality will be affected. | D if RESET=GND by design; B otherwise |
| CMPOUT | 6 | Comparator output is stuck low. | B |
| IN- | 7 | In high-side configuration, a short from the bus supply to GND will occur. High current will flow from bus supply to ground. In low-side configuration, normal operation. | B for high-side or D for low-side |
| IN+ | 8 | In high-side configuration, a short from the bus supply to GND will occur. High current will flow from bus supply to ground. In low-side configuration, input pins are shorted. | B |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| VS | 1 | No power supply to device. Device may be biased through inputs. Output will be close to GND. | B |
| OUT | 2 | Output can be left open, there is no effect on the IC. | B |
| CMPIN | 3 | Comparator input is not defined. | B |
| GND | 4 | GND is floating. Output will be incorrect as it is no longer referenced to GND. | B |
| RESET | 5 | Comparator is in Transparant Mode. If intended connection is not open or GND, functionality will be affected. | D if RESET=open OR GND by design; B otherwise |
| CMPOUT | 6 | Pin can be left open if not needed. | D if CMPOUT=open by design; B otherwise |
| IN- | 7 | Differential input voltage is not well defined. | B |
| IN+ | 8 | Differential input voltage is not well defined. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| VS | 1 | OUT | Output shorts to supply. When left in this configuration for a long time, under high supplies self heating could cause dice junction temperature to exceed 150 degrees Celsius. | B |
| OUT | 2 | CMPIN | Comaprator will be damaged if OUT is higher than the smaller of 5.5 V or VS. | A if OUT is higher than the smaller of 5.5 V or VS; B otherwise |
| CMPIN | 3 | GND | Comparator output is stuck low output is stuck low. | B |
| GND | 4 | RESET | Comparator is in Transparant Mode. If intended connection is not GND or open, functionality will be affected. | D if RESET=GND OR open by design; B otherwise |
| RESET | 5 | CMPOUT | Comparator output is unpredictable. | B |
| CMPOUT | 6 | IN- | In high-side configuration, CMPOUT tied to VBUS, which could exceed Abs Max ratings. Device could be damaged. In low-side configuration, CMPOUT output is stuck low. | A for high-side or B for low-side |
| IN- | 7 | IN+ | Input differential voltage = 0 V. | C |
| IN+ | 8 | VS | In high-side configuration, a short from the bus supply to VS will occur. High current will flow from bus supply to VS or vice versa. Device could be damaged. | A for high-side or B for low-side |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| VS | 1 | Normal operation. | D |
| OUT | 2 | Output shorts to supply. When left in this configuration for a long time, under high supplies self heating could cause dice junction temperature to exceed 150 degrees Celsius. | B |
| CMPIN | 3 | Comparator output is stuck high or unpredictable. | B |
| GND | 4 | Power supply shorted to GND. | B |
| RESET | 5 | Comparator is in Latch Mode. If intended connection is not VS, functionality will be affected. | D if RESET=VS by design; B otherwise |
| CMPOUT | 6 | Comparator output is stuck high or unpredictable.. | B |
| IN- | 7 | In high-side configuration, a short from the bus supply to VS will occur. High current will flow from bus supply to VS or vice versa. Device could be damaged. | A for high-side or B for low-side |
| IN+ | 8 | In high-side configuration, a short from the bus supply to VS will occur. High current will flow from bus supply to VS or vice versa. Device could be damaged. | A for high-side or B for low-side |