SFFS372 February   2022 TPS74801-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 VQFN Package
    2. 2.2 VSON Package
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 VQFN Package
    2. 4.2 VSON Package

VSON Package

Figure 4-2 shows the TPS74801-Q1 pin diagram for the VSON package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS74801-Q1 data sheet.

GUID-D04B7955-F7F7-4D26-B460-3875F9B847AD-low.gif Figure 4-2 Pin Diagram (VSON Package)
Table 4-6 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
IN 1 Device does not turn on. No damage to device. B
IN 2 Device does not turn on. No damage to device. B
PG 3 No damage to device. PG functionality does not work. No impact on remaining functionality. B
BIAS 4 No damage to device. Because band gap and control circuits do not power up, output voltage is not regulated and remains low at 0 V. B
EN 5 Device does not turn on. No damage to device. B
GND 6 No Impact. Normal operation. D
SS 7 Quiescent current increases. Device output remains at 0 V. No damage to device. B
FB 8 Loss of functionality, device does not regulate. Output voltage tracks input voltage and equals VIN minus the dropout. No damage to device. B
OUT 9 Device hits current limit state. If the power dissipation is significant, the device hits thermal shutdown state, and may continue to cycle between the two states. Continuously running the device above rated current degrades device reliability. A
OUT 10 Same as pin 9. A
Table 4-7 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
IN 1 Normal operation. Power supply still connected to remaining IN pin (2), however there is a small risk that the bond wire connecting to the remaining IN pin may fuse under heavily loaded conditions. D/A
IN 2 Same as pin 1. D/A
PG 3 No damage to device. PG functionality does not work. No impact on remaining functionality. B
BIAS 4 No damage to device. Because band gap and control circuits do not power up, output voltage is not regulated and remains low at 0 V. B
EN 5 Because the voltage floats to an indeterminate value, the device can disable. B
GND 6 With the reference pin floating, the voltages at the remaining pins are floating as well and the device is not functional. There is a risk of violating the absolute maximum ratings. B/A
SS 7 No impact. Normal operation. Start-up time defaults to 200 μs, approximately. D
FB 8 Loss of functionality. Output pin voltage is not regulated and remains in an indeterminate state. B
OUT 9 No impact. Normal operation. Load still connected to remaining OUT pin (10). There is a small risk that the bond wire connecting to the remaining OUT pin may fuse under heavily loaded conditions. D/A
OUT 10 Same as pin 9. D/A
Table 4-8 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
IN 1 IN No impact. Normal operation. D
IN 2 PG Very high risk of damage to PG pin and device, resulting from excess current drawn when PG open drain becomes low impedance. A
PG 3 BIAS Very high risk of damage to PG pin and device, resulting from excess current drawn when PG open drain becomes low impedance. A
BIAS 4 EN Device remains ON regardless of enable signal value. B
EN 5 GND Device remains OFF regardless of enable signal value. B
GND 6 SS Quiescent current increases. Device output remains at 0 V. No damage to device. B
SS 7 FB The error amplifier output rails to either one of its supplies, and the LDO output is either at 0 V or tracks VIN and equals VIN – dropout. B
FB 8 OUT VOUT is set to VFB = 0.8 V. B
OUT 9 OUT No impact. Normal operation. D
OUT 10 IN Output voltage is not regulated and equals VIN. B
Table 4-9 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
IN 1 No impact. Normal operation. D
IN 2 No impact. Normal operation. D
PG 3 Very high risk of damage to PG pin and device, resulting from excess current drawn when PG open drain becomes low impedance. A
BIAS 4 Can be certain of normal operation only if sufficient dropout (VIN ≥ VOUT + VDO, where VDO = IOUT × (1.6 / 1.5)) and VIN (VIN ≥ 2.7 V) are provided. Device does not turn on for lower values of VIN, and VOUT remains at 0 V. B
EN 5 Device remains ON regardless of enable signal value. B
GND 6 Device does not turn on. B
SS 7 LDO output pin voltage is not regulated and tracks VIN. VOUT equals VIN – dropout. B
FB 8 LDO output pin voltage is not regulated and equals VIN (under no-load conditions). B
OUT 9 Device is not functional, output voltage is not regulated and equals VIN. B
OUT 10 Same as pin 9. B