SFFS267 December 2025 TPS22954-Q1
This section provides a failure mode analysis (FMA) for the pins of the TPS22954-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-3 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Figure 4-1 shows the TPS22954-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS22954-Q1 datasheet.
Figure 4-1 Pin Diagram (Top View)| PIN | I/O | DESCRIPTION | |
|---|---|---|---|
| NO. | NAME | ||
| 1 | IN | I | Switch input. Bypass this input with a ceramic capacitor to GND. |
| 2 | |||
| 3 | BIAS | I | Bias pin and power supply to the device. |
| 4 | EN | I | Active high switch enable or disable input. Also acts as the input UVLO pin. Use external resistor divider to adjust the UVLO level. Do not leave floating. |
| 5 | GND | — | Device ground. |
| 6 | CT | O | VOUT slew rate control. Place ceramic cap from CT to GND to change the VOUT slew rate of the device and limit the inrush current. CT capacitor must be rated to 25V or higher. |
| 7 | PG | O | Power good. This pin is open drain which pulls low when the voltage on EN or SNS (or both) is below the respective VIL level. |
| 8 | SNS | I | Sense pin. Use external resistor divider to adjust the power good level. Do not leave floating. |
| 9 | OUT | O | Switch output. |
| 10 | |||
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN | 1 | The power supply is shorted. | D |
| 2 | |||
| BIAS | 3 | There is no power supply to the device. The device does not pass through voltage to the VOUT pin. | B |
| EN | 4 | The device is disabled. | D |
| GND | 5 | This is the GND pin. The device operates as normal. | D |
| CT | 6 | Grounding this pin prevents the device from turning on and potentially damages the device. | A |
| PG | 7 | Open drain output, is not pulled up if connected to ground. | B |
| SNS | 8 | VIH,SNS is set to 0V, and the PG pin does not function properly. | B |
| OUT | 9 | If the device is enabled, the device does not limit the power supply current and is damaged. | A |
| 10 |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN | 1 | There is no power supply to the device. The device does not pass through voltage to the VOUT pin. | D |
| 2 | |||
| BIAS | 3 | There is no power supply to the device. The device does not pass through voltage to the VOUT pin. | B |
| EN | 4 | The ON pin potentially floats high or low, the state of the output is unknown. | B |
| GND | 5 | There is no GND connection to the device. The device is not functional. | B |
| CT | 6 | Opening this pin quickens the output rise time if a CT capacitor is attached. | C |
| PG | 7 | The power-good signal is disconnected from the system. | D |
| SNS | 8 | The VIH,SNS setting and the state of the PG pin are unknown. | B |
| OUT | 9 | The output does not deliver the voltage to the load. | D |
| 10 |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| IN | 1 | BIAS | A stronger supply powers the IN and BIAS pins. The operation of the device is potentially affected, however, there is no damage to the device. | B |
| 2 | ||||
| BIAS | 3 | EN | The device is enabled if the BIAS power supply is above the ON threshold (VIH). | D |
| EN | 4 | GND | The device is disabled. | D |
| CT | 6 | PG | Connecting these pins prevents the device from turning on and potentially damages the device. | A |
| PG | 7 | SNS | The PG pin threshold varies, there is no damage to the device. | B |
| SNS | 8 | OUT | The VIH,SNS is set to VOUT. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN | 1 | The device operates normally, as expected. | D |
| 2 | |||
| EN | 3 | The device is enabled if the power supply is above the ON threshold (VIH). | D |
| BIAS | 4 | The device operates normally, as expected. | D |
| GND | 5 | The power supply is shorted. | D |
| CT | 6 | Biasing the CT pin can potentially damage the device. | A |
| PG | 7 | The PG pin potentially pulls too much current from the supply and damages the device. | A |
| SNS | 8 | The VIH,SNS is set to the supply voltage. | B |
| OUT | 9 | The power MOSFET is shorted. Disabling the device no longer blocks power to the VOUT pin. | B |
| 10 |